<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  Using two pn7150 on the same imx6sx board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-two-pn7150-on-the-same-imx6sx-board/m-p/1036507#M152820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi long&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/432602"&gt;NFC in Android Lollipop 5.0.0&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343207"&gt;https://community.nxp.com/docs/DOC-343207&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jan 2020 23:35:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-01-06T23:35:16Z</dc:date>
    <item>
      <title>Using two pn7150 on the same imx6sx board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-two-pn7150-on-the-same-imx6sx-board/m-p/1036506#M152819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all，&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Because of the application needs, we need to use two pn7150 on the same imx6sx board. Can this be achieved through libnfc NCI?Or other implementation methods.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2020 10:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-two-pn7150-on-the-same-imx6sx-board/m-p/1036506#M152819</guid>
      <dc:creator>longh</dc:creator>
      <dc:date>2020-01-06T10:25:58Z</dc:date>
    </item>
    <item>
      <title>Re:  Using two pn7150 on the same imx6sx board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-two-pn7150-on-the-same-imx6sx-board/m-p/1036507#M152820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi long&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/432602"&gt;NFC in Android Lollipop 5.0.0&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343207"&gt;https://community.nxp.com/docs/DOC-343207&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2020 23:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-two-pn7150-on-the-same-imx6sx-board/m-p/1036507#M152820</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-06T23:35:16Z</dc:date>
    </item>
  </channel>
</rss>