<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Is it possible to have a command prompt while flashing?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-have-a-command-prompt-while-flashing/m-p/1036264#M152795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you perform flashing the image the board is running a Linux with reduced options. &lt;BR /&gt;And it is not designed for command prompt.&lt;BR /&gt;However you can try to add "bash" to the end of list of the command in ucl2.xml file (instead of umounting rootfs, etc).&lt;BR /&gt;Then mfg-tool will starn this bash listening to UART and you can close the programm and attach a terminal to this UART.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2019 08:13:04 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-11-26T08:13:04Z</dc:date>
    <item>
      <title>Is it possible to have a command prompt while flashing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-have-a-command-prompt-while-flashing/m-p/1036263#M152794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using imx6sllevk with Yocto bsp and once booting is completed i get a login prompt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6sllevk login# root&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to get this command prompt when it is in flash mode that is after loading the u-boot zImage and dtb.&lt;/P&gt;&lt;P&gt;What changes do I need to make in the ucl2.xml file to give a login prompt?&lt;/P&gt;&lt;P&gt;Also I'm flashing to emmc and please note using sd car for flashing is not an option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 04:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-have-a-command-prompt-while-flashing/m-p/1036263#M152794</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2019-11-26T04:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to have a command prompt while flashing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-have-a-command-prompt-while-flashing/m-p/1036264#M152795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you perform flashing the image the board is running a Linux with reduced options. &lt;BR /&gt;And it is not designed for command prompt.&lt;BR /&gt;However you can try to add "bash" to the end of list of the command in ucl2.xml file (instead of umounting rootfs, etc).&lt;BR /&gt;Then mfg-tool will starn this bash listening to UART and you can close the programm and attach a terminal to this UART.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 08:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-have-a-command-prompt-while-flashing/m-p/1036264#M152795</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-11-26T08:13:04Z</dc:date>
    </item>
  </channel>
</rss>