<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LIN support in IMX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LIN-support-in-IMX/m-p/1034407#M152600</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wasim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6 devices do not support LIN in physical layer as they don't provide PHY. However, the UART module can be configured to 13-bit and it will be able to work as LIN in Data-Link layer, then you only need to connect with external LIN PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Mar 2020 14:46:02 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-03-31T14:46:02Z</dc:date>
    <item>
      <title>LIN support in IMX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIN-support-in-IMX/m-p/1034406#M152599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any LIN driver support in imx? Is it SPI based or UART based?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2020 12:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIN-support-in-IMX/m-p/1034406#M152599</guid>
      <dc:creator>wasim_nazir</dc:creator>
      <dc:date>2020-03-30T12:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: LIN support in IMX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIN-support-in-IMX/m-p/1034407#M152600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wasim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6 devices do not support LIN in physical layer as they don't provide PHY. However, the UART module can be configured to 13-bit and it will be able to work as LIN in Data-Link layer, then you only need to connect with external LIN PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2020 14:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIN-support-in-IMX/m-p/1034407#M152600</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-03-31T14:46:02Z</dc:date>
    </item>
  </channel>
</rss>