<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SLIC voice data receiving on iMx6 using ALSA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SLIC-voice-data-receiving-on-iMx6-using-ALSA/m-p/1034173#M152593</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using iMx6q and trying to read data from phone input and SLIC IC. The IC is giving proper 8-bit Mu Law data at its DTX pin. The communication protocol between is I2S and is operating with parameters PCLK=512kHz and FSync=8kHz. The processor is the master, and I am using ALSA subset utilities (aplay.c userspace application C code) to read and write data on the PCM bus. The ALSA program has a set macro of MU_LAW and a predefined function of snd_pcm_mmap_readi() which has a different way of dealing with pcm areas. The 32-bit word from the PCM channel should be masked out as a 8-bit data via the I2S protocol. How do I modify the ALSA driver so that telephonic data can be read continuously, and fed into the ALSA ring buffer? Is the MU_LAW macro able to receive the 8-bit data properly? Has iMx6q ever been interfaced with SLIC before using ALSA/Linux? If yes, how were the timing diagram matched? Hi, I am using iMx6q and trying to read data from phone input and SLIC IC. The IC is giving proper 8-bit Mu Law data at its DTX pin. The communication protocol between is I2S and is operating with parameters PCLK=512kHz and FSync=8kHz. The processor is the master, and I am using ALSA subset utilities (aplay.c userspace application C code) to read and write data on the PCM bus. The ALSA program has a set macro of MU_LAW and a predefined function of snd_pcm_mmap_readi() which has a different way of dealing with pcm areas. The 32-bit word from the PCM channel should be masked out as a 8-bit data via the I2S protocol. How do I modify the ALSA driver so that telephonic data can be read continuously, and fed into the ALSA ring buffer? Is the MU_LAW macro able to receive the 8-bit data properly? Has iMx6q ever been interfaced with SLIC before using ALSA/Linux? If yes, how were the timing diagram matched? (Please don't share any documentation as a reply. I have been studying every single reference manual of NXP for the past year, and have got idea of SSI, fsl-dai, audio clocking and PCM timing diagrams. I have referred to the ref manual like completely and reached upto here.) (Please don't share any documentation as a reply. I have been studying every single reference manual of NXP for the past year, and have got idea of SSI, fsl-dai, audio clocking and PCM timing diagrams. I have referred to the ref manual like completely and reached upto here.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Mar 2020 05:42:36 GMT</pubDate>
    <dc:creator>abhijeet_ghodga</dc:creator>
    <dc:date>2020-03-02T05:42:36Z</dc:date>
    <item>
      <title>SLIC voice data receiving on iMx6 using ALSA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SLIC-voice-data-receiving-on-iMx6-using-ALSA/m-p/1034173#M152593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using iMx6q and trying to read data from phone input and SLIC IC. The IC is giving proper 8-bit Mu Law data at its DTX pin. The communication protocol between is I2S and is operating with parameters PCLK=512kHz and FSync=8kHz. The processor is the master, and I am using ALSA subset utilities (aplay.c userspace application C code) to read and write data on the PCM bus. The ALSA program has a set macro of MU_LAW and a predefined function of snd_pcm_mmap_readi() which has a different way of dealing with pcm areas. The 32-bit word from the PCM channel should be masked out as a 8-bit data via the I2S protocol. How do I modify the ALSA driver so that telephonic data can be read continuously, and fed into the ALSA ring buffer? Is the MU_LAW macro able to receive the 8-bit data properly? Has iMx6q ever been interfaced with SLIC before using ALSA/Linux? If yes, how were the timing diagram matched? Hi, I am using iMx6q and trying to read data from phone input and SLIC IC. The IC is giving proper 8-bit Mu Law data at its DTX pin. The communication protocol between is I2S and is operating with parameters PCLK=512kHz and FSync=8kHz. The processor is the master, and I am using ALSA subset utilities (aplay.c userspace application C code) to read and write data on the PCM bus. The ALSA program has a set macro of MU_LAW and a predefined function of snd_pcm_mmap_readi() which has a different way of dealing with pcm areas. The 32-bit word from the PCM channel should be masked out as a 8-bit data via the I2S protocol. How do I modify the ALSA driver so that telephonic data can be read continuously, and fed into the ALSA ring buffer? Is the MU_LAW macro able to receive the 8-bit data properly? Has iMx6q ever been interfaced with SLIC before using ALSA/Linux? If yes, how were the timing diagram matched? (Please don't share any documentation as a reply. I have been studying every single reference manual of NXP for the past year, and have got idea of SSI, fsl-dai, audio clocking and PCM timing diagrams. I have referred to the ref manual like completely and reached upto here.) (Please don't share any documentation as a reply. I have been studying every single reference manual of NXP for the past year, and have got idea of SSI, fsl-dai, audio clocking and PCM timing diagrams. I have referred to the ref manual like completely and reached upto here.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 05:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SLIC-voice-data-receiving-on-iMx6-using-ALSA/m-p/1034173#M152593</guid>
      <dc:creator>abhijeet_ghodga</dc:creator>
      <dc:date>2020-03-02T05:42:36Z</dc:date>
    </item>
  </channel>
</rss>