<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mmevk android flashing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mmevk-android-flashing/m-p/1032628#M152475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to flash android on already loaded yocto linux imx8mmevk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to run the command ./uuu_imx_android_flash.sh -f imx8mm, it repeatedly loops in flashing u-boot.imx&lt;/P&gt;&lt;P&gt;and on the debug console I am getting this error:&lt;/P&gt;&lt;P&gt;U-Boot 2018.03 (Nov 29 2019 - 14:44:32 +0530)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MM rev1.0 1500 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 54C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: FSL i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x30a30000&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage select!&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 84a79ee&lt;BR /&gt;- U-Boot 2018.03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net:&lt;BR /&gt;Error: ethernet@30be0000 address not set.&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;Block device mmc 0 not supported&lt;BR /&gt;bcb_rw_block, get_block_size return 0&lt;BR /&gt;read_bootctl, bcb_rw_block read failed&lt;BR /&gt;read command failed&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for uuu&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;dev_get_parent_platdata: null device&lt;BR /&gt;"Synchronous Abort" handler, esr 0x8a000000&lt;BR /&gt;elr: ffffffff802cefff lr : 000000004022dda4 (reloc)&lt;BR /&gt;elr: ffffffffffffffff lr : 00000000bff5eda4&lt;BR /&gt;x0 : 0000000000000000 x1 : 00000000b9f29330&lt;BR /&gt;x2 : 0000000000000001 x3 : ffffffffffffffff&lt;BR /&gt;x4 : aaaaaaaaaaaaaaaa x5 : 0000000000000010&lt;BR /&gt;x6 : 00000000bff5b100 x7 : 00000000bffa17e0&lt;BR /&gt;x8 : 00000000ffffffd0 x9 : 0000000000000008&lt;BR /&gt;x10: 00000000000000cd x11: 000000000000000d&lt;BR /&gt;x12: 0000000000000006 x13: 0000000000000000&lt;BR /&gt;x14: 0000000000000000 x15: 00000000bff32388&lt;BR /&gt;x16: 0000000000000000 x17: 0000000000000000&lt;BR /&gt;x18: 00000000b9f30da8 x19: 00000000b9f29330&lt;BR /&gt;x20: 0000000000000001 x21: 00000000b9f2939f&lt;BR /&gt;x22: 0000000000000000 x23: 000000000000001d&lt;BR /&gt;x24: 0000000000000000 x25: 0000000080000000&lt;BR /&gt;x26: 0000000000000000 x27: 00000000b9f35640&lt;BR /&gt;x28: 0000000000000000 x29: 00000000b9f292d0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Resetting CPU ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;resetting ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Requesting help on this! Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 07:51:06 GMT</pubDate>
    <dc:creator>rajvi_kamdar</dc:creator>
    <dc:date>2019-12-11T07:51:06Z</dc:date>
    <item>
      <title>imx8mmevk android flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mmevk-android-flashing/m-p/1032628#M152475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to flash android on already loaded yocto linux imx8mmevk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I try to run the command ./uuu_imx_android_flash.sh -f imx8mm, it repeatedly loops in flashing u-boot.imx&lt;/P&gt;&lt;P&gt;and on the debug console I am getting this error:&lt;/P&gt;&lt;P&gt;U-Boot 2018.03 (Nov 29 2019 - 14:44:32 +0530)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MM rev1.0 1500 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 54C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: FSL i.MX8MM EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x52 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x30a30000&lt;BR /&gt;tcpc_init: Can't find device id=0x52&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-19&lt;BR /&gt;tcpc_init: Can't find device id=0x50&lt;BR /&gt;setup_typec: tcpc port1 init failed, err=-19&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage select!&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 84a79ee&lt;BR /&gt;- U-Boot 2018.03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net:&lt;BR /&gt;Error: ethernet@30be0000 address not set.&lt;BR /&gt;No ethernet found.&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;Block device mmc 0 not supported&lt;BR /&gt;bcb_rw_block, get_block_size return 0&lt;BR /&gt;read_bootctl, bcb_rw_block read failed&lt;BR /&gt;read command failed&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for uuu&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;dev_get_parent_platdata: null device&lt;BR /&gt;"Synchronous Abort" handler, esr 0x8a000000&lt;BR /&gt;elr: ffffffff802cefff lr : 000000004022dda4 (reloc)&lt;BR /&gt;elr: ffffffffffffffff lr : 00000000bff5eda4&lt;BR /&gt;x0 : 0000000000000000 x1 : 00000000b9f29330&lt;BR /&gt;x2 : 0000000000000001 x3 : ffffffffffffffff&lt;BR /&gt;x4 : aaaaaaaaaaaaaaaa x5 : 0000000000000010&lt;BR /&gt;x6 : 00000000bff5b100 x7 : 00000000bffa17e0&lt;BR /&gt;x8 : 00000000ffffffd0 x9 : 0000000000000008&lt;BR /&gt;x10: 00000000000000cd x11: 000000000000000d&lt;BR /&gt;x12: 0000000000000006 x13: 0000000000000000&lt;BR /&gt;x14: 0000000000000000 x15: 00000000bff32388&lt;BR /&gt;x16: 0000000000000000 x17: 0000000000000000&lt;BR /&gt;x18: 00000000b9f30da8 x19: 00000000b9f29330&lt;BR /&gt;x20: 0000000000000001 x21: 00000000b9f2939f&lt;BR /&gt;x22: 0000000000000000 x23: 000000000000001d&lt;BR /&gt;x24: 0000000000000000 x25: 0000000080000000&lt;BR /&gt;x26: 0000000000000000 x27: 00000000b9f35640&lt;BR /&gt;x28: 0000000000000000 x29: 00000000b9f292d0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Resetting CPU ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;resetting ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Requesting help on this! Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 07:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mmevk-android-flashing/m-p/1032628#M152475</guid>
      <dc:creator>rajvi_kamdar</dc:creator>
      <dc:date>2019-12-11T07:51:06Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mmevk android flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mmevk-android-flashing/m-p/1032629#M152476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; It seems that uboot is failing to initialize the type-C in the board,&amp;nbsp; you can try removing from the defconfig and from the dts file those dependencies:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From defconfig:&lt;/P&gt;&lt;P&gt;CONFIG_USB_TCPC = n&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fsl-imx8mm-evk.dts:&lt;/P&gt;&lt;P&gt;&amp;amp;usbotg1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;drm_mode= "otg";&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;extcon = &amp;lt;0&amp;gt;, &amp;lt;&amp;amp;typec1_ptn5110&amp;gt;;&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;picophy,pre-emp-curr-control = &amp;lt;3&amp;gt;;&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;picophy,dc-vol-level-adjust = &amp;lt;7&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;&amp;amp;usbotg2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;drm_mode= "otg";&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;extcon = &amp;lt;0&amp;gt;, &amp;lt;&amp;amp;typec2_ptn5110&amp;gt;;&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;picophy,pre-emp-curr-control = &amp;lt;3&amp;gt;;&lt;/P&gt;&lt;P&gt;--- &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;picophy,dc-vol-level-adjust = &amp;lt;7&amp;gt;; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aldo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 00:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mmevk-android-flashing/m-p/1032629#M152476</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2019-12-13T00:06:24Z</dc:date>
    </item>
  </channel>
</rss>