<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Control Register configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Control-Register-configuration/m-p/1032154#M152380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dhanush&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for i.MX6UL gpio control one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381277"&gt;Simple GPIO Example - quandry&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Feb 2020 22:55:02 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-02-16T22:55:02Z</dc:date>
    <item>
      <title>Control Register configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Control-Register-configuration/m-p/1032153#M152379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the imx6ul evk board with yocto 4.9.x version ,since i need more number of gpio's I'm tring to mux the ethernet pins ,what value need to be set in the control register, so that the pin gets toggled with the voltage 0 and 3.3v when the&amp;nbsp; pin is made low and high respectively&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Feb 2020 10:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Control-Register-configuration/m-p/1032153#M152379</guid>
      <dc:creator>dhanushvenugopa</dc:creator>
      <dc:date>2020-02-15T10:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: Control Register configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Control-Register-configuration/m-p/1032154#M152380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dhanush&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for i.MX6UL gpio control one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381277"&gt;Simple GPIO Example - quandry&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Feb 2020 22:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Control-Register-configuration/m-p/1032154#M152380</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-16T22:55:02Z</dc:date>
    </item>
  </channel>
</rss>