<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic about Internal POR in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-Internal-POR/m-p/1030397#M152193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hello,Community&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of Internal POR, is the release timing of the reset inside the CPU when both VDD_ARM_IN and VDD_SOC_IN are supplied?&lt;BR /&gt;In the case of BOOT with QuadSPI (QSPI) flash, what is the delay time from the supply of both VDD_ARM_IN and VDD_SOC_IN to the start of access to flash?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Excerpt from i.MX 7Dual Applications Processor Reference Manual&lt;/P&gt;&lt;P&gt;6.2.5.2 Internal POR&lt;BR /&gt;If the external SRC_POR_B signal is not used (always held high or left unconnected), the processor defaults to the internal POR function (PMU controls generation of the POR based on the power supplies).&lt;BR /&gt;If the internal POR function is used, the following power supply requirements must be met:&lt;BR /&gt;• VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source, or&lt;BR /&gt;• VDD_SOC_IN can be supplied before VDD_ARM_IN with a maximum delay of 1ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;Goto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Mar 2020 04:36:04 GMT</pubDate>
    <dc:creator>goto11</dc:creator>
    <dc:date>2020-03-30T04:36:04Z</dc:date>
    <item>
      <title>about Internal POR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-Internal-POR/m-p/1030397#M152193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hello,Community&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of Internal POR, is the release timing of the reset inside the CPU when both VDD_ARM_IN and VDD_SOC_IN are supplied?&lt;BR /&gt;In the case of BOOT with QuadSPI (QSPI) flash, what is the delay time from the supply of both VDD_ARM_IN and VDD_SOC_IN to the start of access to flash?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Excerpt from i.MX 7Dual Applications Processor Reference Manual&lt;/P&gt;&lt;P&gt;6.2.5.2 Internal POR&lt;BR /&gt;If the external SRC_POR_B signal is not used (always held high or left unconnected), the processor defaults to the internal POR function (PMU controls generation of the POR based on the power supplies).&lt;BR /&gt;If the internal POR function is used, the following power supply requirements must be met:&lt;BR /&gt;• VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source, or&lt;BR /&gt;• VDD_SOC_IN can be supplied before VDD_ARM_IN with a maximum delay of 1ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: inherit;"&gt;Goto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2020 04:36:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-Internal-POR/m-p/1030397#M152193</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2020-03-30T04:36:04Z</dc:date>
    </item>
    <item>
      <title>Re: about Internal POR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-Internal-POR/m-p/1030398#M152194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Goto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;In the case of Internal POR, is the release timing of the reset inside the CPU when &lt;BR /&gt;&amp;gt;both VDD_ARM_IN and VDD_SOC_IN are supplied?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general yes. However please note that "Internal POR" case was not validated&lt;BR /&gt;and not recommended in practice, recommended to use option with externally provided&lt;BR /&gt;POR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;In the case of BOOT with QuadSPI (QSPI) flash, what is the delay time from the supply &lt;BR /&gt;&amp;gt;of both VDD_ARM_IN and VDD_SOC_IN to the start of access to flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Such delay is not specificed, as it depends on many factors. Please refer to below&lt;BR /&gt;part of Reference Manual describing reset timings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101103iE1A374956C32CDA7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2020 05:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-Internal-POR/m-p/1030398#M152194</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-03-30T05:39:35Z</dc:date>
    </item>
  </channel>
</rss>