<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCHIP SELECT DISPLAY CONTROLLER</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029566#M152100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HELLO ALL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're Looking For Right SoC For Current Working Project Of Automotive Display Controller. According To SOR From OEM Target Display May Be Either Of Portrait Type And Landscape Type TFT LCD Base Display. As To Landscape Here's No Issue For The System Design But To Portrait Type Due To Almost Of Display Are Landscape Display (Only Few Designs For Vertical Use From Some Panel Maker) So We Need SoC With Enough Performance To Do:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. With Built-in Display Control Unit (IPU) Support Inversion / Flip / Rotate For 90 / 180 Degree To Transform Horizontal Line Into Vertical Which Means Target Design Requires Enough On-Chip Display Framebuffer / Can Allow DMA By Means Of DDR As Framebuffer To&amp;nbsp;Implement For Resolution 720P / 1080P 60FPS.&lt;/P&gt;&lt;P&gt;2. Data Rate Bandwith May Be A Crucial Factor.&lt;/P&gt;&lt;P&gt;3. Enough Performance For Video Overlay (Video Over Video At 720P / 1080P Each 60FPS) (Support 3 Layer Video Captures By MIPI CSI-2)&lt;/P&gt;&lt;P&gt;4. The Key Use Of The Design Is Just For Display Control / Video Control With Overlay Feature PIP / POP (OSD Level) / Video Over Video With Some Communication Functions By Peripherals USB / UART CAN / I2S Codec For Audio Routing Bypass Model / Ethernet.&lt;/P&gt;&lt;P&gt;5. Target System Will Be Legacy Linux.&lt;/P&gt;&lt;P&gt;6. Considering Cost Chip Should Be Lower Than 20$&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our Candidate SoC Is I.MX6 Solo / Solo Plus. My Question Is Can I.MX6 Solo Performs Well For My Requirement?&lt;/P&gt;&lt;P&gt;Note The Target Design Is Just A Display Control Unit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Dec 2019 13:38:53 GMT</pubDate>
    <dc:creator>alighieri</dc:creator>
    <dc:date>2019-12-31T13:38:53Z</dc:date>
    <item>
      <title>CHIP SELECT DISPLAY CONTROLLER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029566#M152100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HELLO ALL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're Looking For Right SoC For Current Working Project Of Automotive Display Controller. According To SOR From OEM Target Display May Be Either Of Portrait Type And Landscape Type TFT LCD Base Display. As To Landscape Here's No Issue For The System Design But To Portrait Type Due To Almost Of Display Are Landscape Display (Only Few Designs For Vertical Use From Some Panel Maker) So We Need SoC With Enough Performance To Do:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. With Built-in Display Control Unit (IPU) Support Inversion / Flip / Rotate For 90 / 180 Degree To Transform Horizontal Line Into Vertical Which Means Target Design Requires Enough On-Chip Display Framebuffer / Can Allow DMA By Means Of DDR As Framebuffer To&amp;nbsp;Implement For Resolution 720P / 1080P 60FPS.&lt;/P&gt;&lt;P&gt;2. Data Rate Bandwith May Be A Crucial Factor.&lt;/P&gt;&lt;P&gt;3. Enough Performance For Video Overlay (Video Over Video At 720P / 1080P Each 60FPS) (Support 3 Layer Video Captures By MIPI CSI-2)&lt;/P&gt;&lt;P&gt;4. The Key Use Of The Design Is Just For Display Control / Video Control With Overlay Feature PIP / POP (OSD Level) / Video Over Video With Some Communication Functions By Peripherals USB / UART CAN / I2S Codec For Audio Routing Bypass Model / Ethernet.&lt;/P&gt;&lt;P&gt;5. Target System Will Be Legacy Linux.&lt;/P&gt;&lt;P&gt;6. Considering Cost Chip Should Be Lower Than 20$&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our Candidate SoC Is I.MX6 Solo / Solo Plus. My Question Is Can I.MX6 Solo Performs Well For My Requirement?&lt;/P&gt;&lt;P&gt;Note The Target Design Is Just A Display Control Unit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Dec 2019 13:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029566#M152100</guid>
      <dc:creator>alighieri</dc:creator>
      <dc:date>2019-12-31T13:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: CHIP SELECT DISPLAY CONTROLLER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029567#M152101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bright&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in general these requirements are feasible, one can test&lt;/P&gt;&lt;P&gt;performance with i.MX6DL Sabre SD board using Demo Images from&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW" title="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW"&gt;i.MX Software and Development Tools | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for rotation may be useful to check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/303359"&gt;90 degree or 270 degree rotation not working using fb0 rotate?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jan 2020 10:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029567#M152101</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-01T10:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: CHIP SELECT DISPLAY CONTROLLER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029568#M152102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HELLO IGOR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANK YOU FOR YOUR REPLY TO MY QUESTION. IN FACT I NOW IPU CAN SUPPORT DISPLAY &lt;A href="http://cache.freescale.com/files/training/doc/ftf/2014/FTF-CON-F0119.pdf"&gt;ORIENTATION INVERSION&lt;/A&gt;&amp;nbsp;(SEE HERE PRESENTATION TO INTRODUCE IPUv3H) BUT I’M NOT SURE OF ENOUGH PERFORMANCE FOR TARGET RESOLUTION / FRAMERATE AND ALSO ANOTHER USE CASE OF VIDEO OVERLAY. THAT’ WHY I POSTED HERE TO ASK FOR EXPERT OPINIONS. CAN YOU HELP TO CHECK:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1. Here Are 2 Requirements. One For&amp;nbsp;Display Orientation Conversion (Flip / Rotate) Another For Video Overlay.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-1.&amp;nbsp;We Have No Doubt About The Display Rotation Capability Of IPU But Wonder:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-1-1. Support Maximum Resolution&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-1-2. Support Maximum Framerate&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-1-3. Support Maximum Frame Buffer Size (Display)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-2. About Overlay We Know PXP Can Do Image Color Key For Alpha Transparency Use Case Also PIP (Picture In Picture) / POP (Picture Over Picture) But Have No Idea About Video Overlay Capability:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101400i0186D024F9215241/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-2-1. Support Maximum Frame Buffer Size (Camera In)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1-2-2. Support Maximum Bandwidth (Data Rate)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;For Our Use Case We May Need Support 2 - 3 Video Input Overlay:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Each Reasolution May Be Either Of:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1024*768&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1280*720&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;1920*1080&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;@ Framerate 60FPS&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;Two&amp;nbsp;Of Video Input From MIPI CSI-2 Along With Renesas (Intersil) TW8844/45&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Left One May From Ethernet Stream.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;IN CONLUSION OF WHAT I ASKED HERE&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;THE MOST IMPORTANT OF ALL:&lt;/P&gt;&lt;P&gt;ROTATE 90 / 180 DEGREE (DISPLAY / CAMERA)&lt;/P&gt;&lt;P&gt;720P / 1080P @ FRAMERATE 60FPS&lt;/P&gt;&lt;P&gt;MEANWHILE&lt;/P&gt;&lt;P&gt;SUPPORT VIDEO OVERLAY&lt;/P&gt;&lt;P&gt;EACH VIDEO INPUT FROM MIPI CSI-2 (PARALLEL)&lt;/P&gt;&lt;P&gt;720P / 1080P @ FRAMRATE 60FPS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;KEY FACTOR&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;FRAMEBUFFER SIZE&lt;/P&gt;&lt;P&gt;DISPLAY FRAME BUFFER&lt;/P&gt;&lt;P&gt;CAMERA FRAME BUFFER&lt;/P&gt;&lt;P&gt;DATA TRANSMISSION BANDWIDTH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRIGHT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2020 02:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029568#M152102</guid>
      <dc:creator>alighieri</dc:creator>
      <dc:date>2020-01-02T02:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: CHIP SELECT DISPLAY CONTROLLER</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029569#M152103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HELLO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'M STILL LOOKING FOR ANSWERS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Our Case We Need 2-Way Video Input Each With Resolution 720P @ Frame Rate 60FPS In The Meantime To Overlay Together By Using Stream Mode And MEMCPY To IPU's Frame Buffer For 90 Degree Rotation. Is That Possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2020 11:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CHIP-SELECT-DISPLAY-CONTROLLER/m-p/1029569#M152103</guid>
      <dc:creator>alighieri</dc:creator>
      <dc:date>2020-01-14T11:34:41Z</dc:date>
    </item>
  </channel>
</rss>