<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVerifying images in HAB in Linux or OPTEE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029061#M152042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to work on an update procedure on an IMX6UL that checks to see if an image will pass the HAB check before updating the images. I'm having trouble accessing the boot ROM from OPTEE so I need to re-implement the authentication function in as a TA in OPTEE or failing that as a regular Linux application, similar to the uboot command hab_auth_img. Is there any code available for this? Is there a way to make the CST do this? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Feb 2020 23:38:25 GMT</pubDate>
    <dc:creator>nicholash</dc:creator>
    <dc:date>2020-02-13T23:38:25Z</dc:date>
    <item>
      <title>Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029061#M152042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to work on an update procedure on an IMX6UL that checks to see if an image will pass the HAB check before updating the images. I'm having trouble accessing the boot ROM from OPTEE so I need to re-implement the authentication function in as a TA in OPTEE or failing that as a regular Linux application, similar to the uboot command hab_auth_img. Is there any code available for this? Is there a way to make the CST do this? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 23:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029061#M152042</guid>
      <dc:creator>nicholash</dc:creator>
      <dc:date>2020-02-13T23:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029062#M152043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, is there any solution this? This seems like a fairly common use case that will stop people bricking their devices. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 00:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029062#M152043</guid>
      <dc:creator>nicholash</dc:creator>
      <dc:date>2020-02-18T00:50:20Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029063#M152044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; I've sent You directly some considerations. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 06:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1029063#M152044</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-02-26T06:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1231901#M169599</link>
      <description>&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;I'm trying to use hab checking function for imxull in kernel userspace is there any implementation?&lt;/P&gt;&lt;P&gt;Can you share your considerations?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I would like to achive is a signature checking&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 07:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1231901#M169599</guid>
      <dc:creator>gcornacchia</dc:creator>
      <dc:date>2021-02-17T07:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1232735#M169656</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183308"&gt;@gcornacchia&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; There is no the&amp;nbsp;&lt;SPAN&gt;hab checking in&amp;nbsp; userspace.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 09:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/1232735#M169656</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-02-18T09:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: Verifying images in HAB in Linux or OPTEE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/2169623#M240726</link>
      <description>&lt;P&gt;We also have the requirement to perform kernel signature verification within OP-TEE. Could you provide the methodology and an implementation (code) for this?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Mon, 15 Sep 2025 09:46:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Verifying-images-in-HAB-in-Linux-or-OPTEE/m-p/2169623#M240726</guid>
      <dc:creator>lijiangning</dc:creator>
      <dc:date>2025-09-15T09:46:53Z</dc:date>
    </item>
  </channel>
</rss>