<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  IMAX8 PCIE_REFCLK100M in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMAX8-PCIE-REFCLK100M/m-p/1027185#M151785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;The IMAX8 PCIE_REFCLK100M can use as a resource for output?or need external clock input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;both options can be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Feb 2020 23:35:53 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-02-27T23:35:53Z</dc:date>
    <item>
      <title>IMAX8 PCIE_REFCLK100M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMAX8-PCIE-REFCLK100M/m-p/1027184#M151784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The IMAX8 PCIE_REFCLK100M can use as a resource for output?or need external clock input.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 17:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMAX8-PCIE-REFCLK100M/m-p/1027184#M151784</guid>
      <dc:creator>ceng_guanghui</dc:creator>
      <dc:date>2020-02-27T17:10:56Z</dc:date>
    </item>
    <item>
      <title>Re:  IMAX8 PCIE_REFCLK100M</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMAX8-PCIE-REFCLK100M/m-p/1027185#M151785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;The IMAX8 PCIE_REFCLK100M can use as a resource for output?or need external clock input.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;both options can be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 23:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMAX8-PCIE-REFCLK100M/m-p/1027185#M151785</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-27T23:35:53Z</dc:date>
    </item>
  </channel>
</rss>