<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto media device ko question in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026174#M151615</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xu Ji,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this problem still present? I would recommend looking at the default kernel configuration files as sometimes there are additional dependencies to the drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you modified the media driver then check with the manufacturer if there are additional dependencies and make sure that the required libraries are also installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Feb 2020 16:47:16 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-02-03T16:47:16Z</dc:date>
    <item>
      <title>Yocto media device ko question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026173#M151614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on i.MX8QM yocto platform,and now I changed some media driver to ko.&lt;/P&gt;&lt;P&gt;CONFIG_GMSL_MAX9286=m&lt;BR /&gt;CONFIG_IMX8_MEDIA_DEVICE=m&lt;BR /&gt;CONFIG_IMX8_JPEG=m&lt;/P&gt;&lt;P&gt;when power on&amp;nbsp;&lt;SPAN&gt;CONFIG_IMX8_MEDIA_DEVICE ko and&amp;nbsp;CONFIG_IMX8_JPEG ko load by systemd,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why camera ko not be load?which service in systemd load the media driver ko?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 05:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026173#M151614</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2020-01-17T05:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto media device ko question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026174#M151615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xu Ji,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this problem still present? I would recommend looking at the default kernel configuration files as sometimes there are additional dependencies to the drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you modified the media driver then check with the manufacturer if there are additional dependencies and make sure that the required libraries are also installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2020 16:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026174#M151615</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-02-03T16:47:16Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto media device ko question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026175#M151616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi，gusarambula&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this problem still present，the media_device module and jpeg module loaded by Udev service,but camera driver module not loaded,do u know why it is like that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2020 01:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-media-device-ko-question/m-p/1026175#M151616</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2020-02-04T01:36:00Z</dc:date>
    </item>
  </channel>
</rss>