<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Does uuu script directly write to NAND flash address?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025756#M151599</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jupiter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;direct programming to nand addresses is not used, please check below links&lt;/P&gt;&lt;P&gt;explaining nand programming with uuu tool&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/517143"&gt;imx6ull burned image to nand by uuu&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wiki.somlabs.com/index.php/How_to_write_image_to_VisionSOM-6ULL_NAND_memory_using_UUU_tool_on_Linux" title="https://wiki.somlabs.com/index.php/How_to_write_image_to_VisionSOM-6ULL_NAND_memory_using_UUU_tool_on_Linux"&gt;How to write image to VisionSOM-6ULL NAND memory using UUU tool on Linux - SomLabs Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 01 Feb 2020 05:19:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-02-01T05:19:55Z</dc:date>
    <item>
      <title>Does uuu script directly write to NAND flash address?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025754#M151597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run ./uuu uuu_ram to install a dtb file to -addr 0x83000000, is that imx6ulz-pmu2.dtb file written to the NAND flash address 0x83000000 or RAM address 0x83000000?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDP: write -f imx6ulz-pmu2.dtb -addr 0x83000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is written to NAND address, How can I check if the file imx6ulz-pmu2.dtb is indeed installed in NAND address 0x83000000?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- jh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 15:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025754#M151597</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2020-01-31T15:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: Does uuu script directly write to NAND flash address?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025755#M151598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, figured out, it is writing to RAM address,&amp;nbsp; how can I take that file from the RAM address 0x83000000 and flash it to NAND? I know there are other alternative to set up MTD partitions, but I like to install files from RAM address to NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Feb 2020 01:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025755#M151598</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2020-02-01T01:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: Does uuu script directly write to NAND flash address?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025756#M151599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jupiter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;direct programming to nand addresses is not used, please check below links&lt;/P&gt;&lt;P&gt;explaining nand programming with uuu tool&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/517143"&gt;imx6ull burned image to nand by uuu&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wiki.somlabs.com/index.php/How_to_write_image_to_VisionSOM-6ULL_NAND_memory_using_UUU_tool_on_Linux" title="https://wiki.somlabs.com/index.php/How_to_write_image_to_VisionSOM-6ULL_NAND_memory_using_UUU_tool_on_Linux"&gt;How to write image to VisionSOM-6ULL NAND memory using UUU tool on Linux - SomLabs Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Feb 2020 05:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025756#M151599</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-01T05:19:55Z</dc:date>
    </item>
    <item>
      <title>Re: Does uuu script directly write to NAND flash address?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025757#M151600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response and link, but that has to use the somlabs complicated source, it was using kernel 4.9 which is also incompatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just need to download one UBI image ubi.image built by ubinize command via uuu, are there any other alternatives?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ sudo ./uuu ubi.image&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Feb 2020 08:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-uuu-script-directly-write-to-NAND-flash-address/m-p/1025757#M151600</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2020-02-01T08:27:10Z</dc:date>
    </item>
  </channel>
</rss>