<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RT1050 10pin JTAG Help</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1050-10pin-JTAG-Help/m-p/1025325#M151523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Kamal&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 10pin connector is for the onboard debugger if you want to program the RT you need to use the 20pin connector.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 01:14:22 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2019-12-11T01:14:22Z</dc:date>
    <item>
      <title>RT1050 10pin JTAG Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1050-10pin-JTAG-Help/m-p/1025324#M151522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the MIMXRT1050 board with Keilv5 IDE and the Segger Arm Flasher with the Jlink 10pin adapter. I have already programmed the board using the 20pin JTAG, but now I am trying the same thing with the 10pin JTAG and it is not working. I try to download to flash as normal and it attempts to download then the board resets and Keil returns "Flash Timeout. Reset the Target and try again." .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the flash configuration, I can see that the board is connected using the Jlink Flasher. Is there anything I need to change with the configuration of the board? Maybe the Jumpers need to be a certain way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kamal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 21:04:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1050-10pin-JTAG-Help/m-p/1025324#M151522</guid>
      <dc:creator>kamal1</dc:creator>
      <dc:date>2019-12-09T21:04:56Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050 10pin JTAG Help</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1050-10pin-JTAG-Help/m-p/1025325#M151523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Kamal&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 10pin connector is for the onboard debugger if you want to program the RT you need to use the 20pin connector.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 01:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1050-10pin-JTAG-Help/m-p/1025325#M151523</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-12-11T01:14:22Z</dc:date>
    </item>
  </channel>
</rss>