<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PDM mic driver (non-Linux) for i.MX8M Mini in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PDM-mic-driver-non-Linux-for-i-MX8M-Mini/m-p/1024757#M151421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Doug&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check MCUXpresso SDK_EVK-MIMX8M Mini (*/driver_examples/pdm folder),&lt;/P&gt;&lt;P&gt;build it on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Mar 2020 23:41:20 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-03-12T23:41:20Z</dc:date>
    <item>
      <title>PDM mic driver (non-Linux) for i.MX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PDM-mic-driver-non-Linux-for-i-MX8M-Mini/m-p/1024756#M151420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A customer would like to use the PDM mic interface on an i.MX8M Mini processor but they cannot use Linux. Therefore they are in need of a driver that is suitable for bare metal or to be used with an RTOS. Has such a driver been developed internally or are you aware of an open source solution that can be leveraged.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is fairly urgent so any input or guidance that can be provided is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Doug Bruce&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 21:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PDM-mic-driver-non-Linux-for-i-MX8M-Mini/m-p/1024756#M151420</guid>
      <dc:creator>nxa14910</dc:creator>
      <dc:date>2020-03-12T21:57:04Z</dc:date>
    </item>
    <item>
      <title>Re: PDM mic driver (non-Linux) for i.MX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PDM-mic-driver-non-Linux-for-i-MX8M-Mini/m-p/1024757#M151421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Doug&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check MCUXpresso SDK_EVK-MIMX8M Mini (*/driver_examples/pdm folder),&lt;/P&gt;&lt;P&gt;build it on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 23:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PDM-mic-driver-non-Linux-for-i-MX8M-Mini/m-p/1024757#M151421</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-03-12T23:41:20Z</dc:date>
    </item>
  </channel>
</rss>