<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Why am I getting a compilation error in menu.c when building LTIB?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-am-I-getting-a-compilation-error-in-menu-c-when-building/m-p/1023991#M151329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manuel Malagon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LTIB have not been updated in a while, which makes it tricky to run on newer Ubuntu distributions. There are some posts that may be of help where they have worked out the package name changes an availability, but I would recommend using an older Ubuntu release if you can. (I understand you may not want to go all the way back to 9.04 but I’ve seen users using LTIB with Ubuntu 12.04, I would try to use 12.04 or 14.04)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-1442"&gt;https://community.nxp.com/docs/DOC-1442&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/263972#264975"&gt;https://community.nxp.com/thread/263972#264975&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could also consider switching to Yocto. Support for the i.MX28 is only provided on the Community BSP which is part of the Yocto Project and thus Open Source and supported by the Community, but it may be of help.&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.github.io/#documentation"&gt;https://freescale.github.io/#documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jan 2020 20:47:44 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-01-31T20:47:44Z</dc:date>
    <item>
      <title>Why am I getting a compilation error in menu.c when building LTIB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-am-I-getting-a-compilation-error-in-menu-c-when-building/m-p/1023990#M151328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm following the steps on &lt;STRONG&gt;page 27&lt;/STRONG&gt; from&amp;nbsp;&lt;STRONG&gt;i.MX28 EVK Linux User’s Guide, Rev. L2.6.35_1.1.0&lt;/STRONG&gt; regarding the&amp;nbsp;Installing and Building of the LTIB and I'm having the process stop with the following error (taken from the log):&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:416: undefined reference to `next_id'&lt;BR /&gt;/opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:427: undefined reference to `next_id'&lt;BR /&gt;collect2: error: ld returned 1 exit status&lt;BR /&gt;Makefile:106: recipe for target 'conf' failed&lt;BR /&gt;make: *** [conf] Error 1&lt;BR /&gt;error: Bad exit status from /home/m4l490n/Projects/ltib/tmp/rpm-tmp.27037 (%build)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;RPM build errors:&lt;BR /&gt; Bad exit status from /home/m4l490n/Projects/ltib/tmp/rpm-tmp.27037 (%build)&lt;BR /&gt;Build time for lkc: 1 seconds&lt;/P&gt;&lt;P&gt;Failed building lkc&lt;BR /&gt;Died at ./ltib line 1392.&lt;BR /&gt;traceback:&lt;BR /&gt; main::build_host_rpms:1392&lt;BR /&gt; main::host_checks:1447&lt;BR /&gt; main:554&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Started: Thu Jan 30 12:48:18 2020&lt;BR /&gt;Ended: Thu Jan 30 12:51:54 2020&lt;BR /&gt;Elapsed: 216 seconds&lt;/P&gt;&lt;P&gt;These packages failed to build:&lt;BR /&gt;lkc&lt;/P&gt;&lt;P&gt;Build Failed&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does anyone know why I'm getting that error? &lt;EM&gt;&lt;STRONG&gt;Do I absolutely need to install&amp;nbsp;Ubuntu 9.04, 9.10, or 10.04 as the document mentions?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I include the complete log in case somebody knows how to do this and can get more information out of the log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the specs for my host computer where I need LTIB:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;OS: Linux Mint 18.3 Sylvia x86_64 &lt;BR /&gt;VMware Virtual Platform None &lt;BR /&gt;Kernel: 4.15.0-76-generic &lt;BR /&gt;Uptime: 22 hours, 29 mins &lt;BR /&gt;Packages: 3278 (dpkg), 5 (flatpak), 6 (snap) &lt;BR /&gt;Shell: zsh 5.1.1 &lt;BR /&gt;Resolution: 2560x1440, 2560x1440 &lt;BR /&gt;DE: Plasma &lt;BR /&gt;WM: KWin &lt;BR /&gt;Theme: Breeze [GTK2/3] &lt;BR /&gt;Icons: breeze [GTK2/3] &lt;BR /&gt;Terminal: gnome-terminal &lt;BR /&gt;CPU: Intel Xeon E3-1505M v6 (4) @ 2.999GHz &lt;BR /&gt;GPU: 00:0f.0 VMware SVGA II Adapter &lt;BR /&gt; Memory: 4012MiB / 7953MiB&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 18:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-am-I-getting-a-compilation-error-in-menu-c-when-building/m-p/1023990#M151328</guid>
      <dc:creator>m4l490n</dc:creator>
      <dc:date>2020-01-30T18:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: Why am I getting a compilation error in menu.c when building LTIB?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-am-I-getting-a-compilation-error-in-menu-c-when-building/m-p/1023991#M151329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manuel Malagon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LTIB have not been updated in a while, which makes it tricky to run on newer Ubuntu distributions. There are some posts that may be of help where they have worked out the package name changes an availability, but I would recommend using an older Ubuntu release if you can. (I understand you may not want to go all the way back to 9.04 but I’ve seen users using LTIB with Ubuntu 12.04, I would try to use 12.04 or 14.04)&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-1442"&gt;https://community.nxp.com/docs/DOC-1442&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/263972#264975"&gt;https://community.nxp.com/thread/263972#264975&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could also consider switching to Yocto. Support for the i.MX28 is only provided on the Community BSP which is part of the Yocto Project and thus Open Source and supported by the Community, but it may be of help.&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.github.io/#documentation"&gt;https://freescale.github.io/#documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 20:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-am-I-getting-a-compilation-error-in-menu-c-when-building/m-p/1023991#M151329</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-01-31T20:47:44Z</dc:date>
    </item>
  </channel>
</rss>