<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: it6251 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023621#M151275</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks !&amp;nbsp;&lt;/P&gt;&lt;P&gt;I solve . Because The reset foot of it6251 is pulled down&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Mar 2020 03:34:19 GMT</pubDate>
    <dc:creator>yuhundehao</dc:creator>
    <dc:date>2020-03-10T03:34:19Z</dc:date>
    <item>
      <title>it6251</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023619#M151273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Board:imx6q&lt;/P&gt;&lt;P&gt;linux kernel :3.0.35&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use it6251 conversion chip to convert LVDS signal into EDP signal. Now the conversion is successful, but there is a problem that the logo display interface is not displayed, and the app startup interface can be displayed normally，why?&lt;/P&gt;&lt;P&gt;I can't even try to initialize the chip by putting it into uboot。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 07:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023619#M151273</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2020-02-27T07:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: it6251</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023620#M151274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuhundehao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to adjust lvds timing parameters in&amp;nbsp;struct fb_videomode using example on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/383078"&gt;IMX6Q drive the LVDS screen ,but can not light up...&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 09:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023620#M151274</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-27T09:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: it6251</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023621#M151275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks !&amp;nbsp;&lt;/P&gt;&lt;P&gt;I solve . Because The reset foot of it6251 is pulled down&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 03:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/it6251/m-p/1023621#M151275</guid>
      <dc:creator>yuhundehao</dc:creator>
      <dc:date>2020-03-10T03:34:19Z</dc:date>
    </item>
  </channel>
</rss>