<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: nxp uuu工具</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023018#M151202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;我指的image是二进制文件，不是单独的uboot kernel。。。比如 dd if=/dev/zero of=./system.img bs=1M count=500，生成一个500M的img文件，然后将其分为2个区，一个为fat，一个为ext4，把dtb、kernel放到fat区，rootfs放到ext4分区，将这个img直接烧录到emmc的UDA，但是dd制作的img无法进行resize2fs操作，问题肯定在img的制作方式上，不知道官方是否有提供制作这种img的方法？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2020 13:55:21 GMT</pubDate>
    <dc:creator>luoyaojun</dc:creator>
    <dc:date>2020-03-13T13:55:21Z</dc:date>
    <item>
      <title>nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023016#M151200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;目前正在学习研究uuu工具对nxp系列平台进行刷机操作，现遇到问题：&lt;/P&gt;&lt;P&gt;uuu可以将image file直接烧写进UDA，那么这个image file如何制作？bitbake似乎无法生成img？&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/101751i40D16D071BC61FC2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;关于LOADADDR的一些疑问，这个LOADADDR的地址如何确定？以IMX6UL为例：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102054iAB815536144F403C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;8000_0000为内存起始地址，理论上我们可以将LOADADDR设定为8000_0000~FFFF_FFFF中的任何位置。&lt;/P&gt;&lt;P&gt;我还接触了一些IMX6UL，它们的LOADDADDR为10008000，请问这否是指将内核加载到AES Encryption区域？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 13:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023016#M151200</guid>
      <dc:creator>luoyaojun</dc:creator>
      <dc:date>2020-03-12T13:38:11Z</dc:date>
    </item>
    <item>
      <title>Re: nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023017#M151201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can get image(uboot, kernel....) though bitbake, for loadaddr, pls find the chapter Table 45. Board-specific default values of enclose file, for more detailed information about this, you can refer to the enclosed file too&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 09:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023017#M151201</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-03-13T09:34:29Z</dc:date>
    </item>
    <item>
      <title>Re: nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023018#M151202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;我指的image是二进制文件，不是单独的uboot kernel。。。比如 dd if=/dev/zero of=./system.img bs=1M count=500，生成一个500M的img文件，然后将其分为2个区，一个为fat，一个为ext4，把dtb、kernel放到fat区，rootfs放到ext4分区，将这个img直接烧录到emmc的UDA，但是dd制作的img无法进行resize2fs操作，问题肯定在img的制作方式上，不知道官方是否有提供制作这种img的方法？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 13:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023018#M151202</guid>
      <dc:creator>luoyaojun</dc:creator>
      <dc:date>2020-03-13T13:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023019#M151203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we have sdcard image which includes dtb kernel and rootfs, you can find the sdcard layout from the link as below, &lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/Freescale/meta-fsl-arm/blob/master/classes/image_types_fsl.bbclass" title="https://github.com/Freescale/meta-fsl-arm/blob/master/classes/image_types_fsl.bbclass"&gt;meta-fsl-arm/image_types_fsl.bbclass at master · Freescale/meta-fsl-arm · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2020 04:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023019#M151203</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-03-17T04:13:56Z</dc:date>
    </item>
    <item>
      <title>Re: nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023020#M151204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;嗯，这是制作sdcard的方法，buildroot中的genimage工具也可以制作这个img文件，但我希望得到emmc.img文件像这样：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99403i4939EC7D6B7F287B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;假设emmc.img制作出来后大小为1G，我使用uuu将该文件烧录到我板子的emmc后可以成功启动（现在已经实现并测试可以启动），进入系统后使用resize2fs无法将剩余空间利用起来：&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;emmc实际使用：&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# df -h&lt;BR /&gt;Filesystem Size Used Avail Use% Mounted on&lt;BR /&gt;/dev/root 1.2G 957M 143M 88% /&lt;BR /&gt;devtmpfs 88M 76K 88M 1% /dev&lt;BR /&gt;tmpfs 40K 0 40K 0% /mnt/.psplash&lt;BR /&gt;tmpfs 249M 216K 249M 1% /run&lt;BR /&gt;tmpfs 249M 88K 249M 1% /var/volatile&lt;BR /&gt;/dev/mmcblk1p1 16M 5.5M 11M 35% /run/media/mmcblk1p1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;emmc总容量：&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# fdisk -l&lt;/P&gt;&lt;P&gt;Disk /dev/mmcblk1: 7.3 GiB, 7801405440 bytes, 15237120 sectors&lt;BR /&gt;Units: sectors of 1 * 512 = 512 bytes&lt;BR /&gt;Sector size (logical/physical): 512 bytes / 512 bytes&lt;BR /&gt;I/O size (minimum/optimal): 512 bytes / 512 bytes&lt;BR /&gt;Disklabel type: dos&lt;BR /&gt;Disk identifier: 0x00000000&lt;/P&gt;&lt;P&gt;Device Boot Start End Sectors Size Id Type&lt;BR /&gt;/dev/mmcblk1p1 * 1 32768 32768 16M c W95 FAT32 (LBA)&lt;BR /&gt;/dev/mmcblk1p2 32769 2678784 2646016 1.3G 83 Linux&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;使用命令resize2fs无法扩展分区：&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@imx6ulevk:~# resize2fs /dev/mmcblk1p2&lt;BR /&gt;resize2fs 1.44.5 (15-Dec-2018)&lt;BR /&gt;The filesystem is already 330752 (4k) blocks long. Nothing to do!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;引起这个故障的原因是否是我的emmc.img有问题？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 14:12:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023020#M151204</guid>
      <dc:creator>luoyaojun</dc:creator>
      <dc:date>2020-03-20T14:12:24Z</dc:date>
    </item>
    <item>
      <title>Re: nxp uuu工具</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023021#M151205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;补充：&lt;/P&gt;&lt;P&gt;EMMC 8G 暂时忽略除UDA以外的分区。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 14:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/nxp-uuu%E5%B7%A5%E5%85%B7/m-p/1023021#M151205</guid>
      <dc:creator>luoyaojun</dc:creator>
      <dc:date>2020-03-20T14:14:04Z</dc:date>
    </item>
  </channel>
</rss>