<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックadb devices not detecting device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adb-devices-not-detecting-device/m-p/1020487#M150929</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed Windows 10 on Virtualbox on a MAC host.&lt;/P&gt;&lt;P&gt;Installed android platform-tools and tools and updated the environment variables.&lt;/P&gt;&lt;P&gt;After this, I have connected the Indigo2 device (imx8mn nano) to the system&lt;/P&gt;&lt;P&gt;Then connected USB device to Windows machine from the menu (Devices&amp;nbsp; -&amp;gt; USB -&amp;gt; Jupiter USB device) as shown in the IMG-5037.jpg&lt;/P&gt;&lt;P&gt;Then opened the Device Manager in the Windows (Virtual system). Scan for new hardwarde as shown in IMG-5038.jpg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here the device is shown. But adb devices is not recognizing the device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After this, I have tried to update the&amp;nbsp; driver using using ADB device driver and also WinUsb Device Driver as shown in IMG-5040.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both cases, I am getting error as "This device cannot start (Code 10) Error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated as I am using this for first time on a fresh installation of Windows 10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if any other information is needed. I am able to connect to serial console to that same Windows machine for console logs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Srini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 00:08:24 GMT</pubDate>
    <dc:creator>srinivas_jakkul</dc:creator>
    <dc:date>2020-01-16T00:08:24Z</dc:date>
    <item>
      <title>adb devices not detecting device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-devices-not-detecting-device/m-p/1020487#M150929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed Windows 10 on Virtualbox on a MAC host.&lt;/P&gt;&lt;P&gt;Installed android platform-tools and tools and updated the environment variables.&lt;/P&gt;&lt;P&gt;After this, I have connected the Indigo2 device (imx8mn nano) to the system&lt;/P&gt;&lt;P&gt;Then connected USB device to Windows machine from the menu (Devices&amp;nbsp; -&amp;gt; USB -&amp;gt; Jupiter USB device) as shown in the IMG-5037.jpg&lt;/P&gt;&lt;P&gt;Then opened the Device Manager in the Windows (Virtual system). Scan for new hardwarde as shown in IMG-5038.jpg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here the device is shown. But adb devices is not recognizing the device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After this, I have tried to update the&amp;nbsp; driver using using ADB device driver and also WinUsb Device Driver as shown in IMG-5040.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both cases, I am getting error as "This device cannot start (Code 10) Error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated as I am using this for first time on a fresh installation of Windows 10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if any other information is needed. I am able to connect to serial console to that same Windows machine for console logs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Srini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 00:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-devices-not-detecting-device/m-p/1020487#M150929</guid>
      <dc:creator>srinivas_jakkul</dc:creator>
      <dc:date>2020-01-16T00:08:24Z</dc:date>
    </item>
    <item>
      <title>Re: adb devices not detecting device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adb-devices-not-detecting-device/m-p/1020488#M150930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="353302" data-username="srinivas_jakkula@whirlpool.com" href="https://community.nxp.com/people/srinivas_jakkula@whirlpool.com"&gt;Srinivas&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Probably, you need to install android ADB driver to windows 10. try it , please!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; you refer to the link to download and install adb driver.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-342719"&gt;https://community.nxp.com/docs/DOC-342719&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 03:05:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adb-devices-not-detecting-device/m-p/1020488#M150930</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-01-16T03:05:15Z</dc:date>
    </item>
  </channel>
</rss>