<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx7ulp RAM error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-RAM-error/m-p/1020403#M150906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I used my imx7ulpevk and replaced the DRAM to a new 4Gb LPDDR3. After changing some code, I can bootup Linux and run "memtester" for DRAM burn in. Then I Run into an error. The error message is kind of lengthy and messy, please refer to the attached file and give some comments for direction of debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ka-Yi Yeh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 06:56:55 GMT</pubDate>
    <dc:creator>kayiyeh</dc:creator>
    <dc:date>2019-11-21T06:56:55Z</dc:date>
    <item>
      <title>imx7ulp RAM error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-RAM-error/m-p/1020403#M150906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I used my imx7ulpevk and replaced the DRAM to a new 4Gb LPDDR3. After changing some code, I can bootup Linux and run "memtester" for DRAM burn in. Then I Run into an error. The error message is kind of lengthy and messy, please refer to the attached file and give some comments for direction of debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ka-Yi Yeh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 06:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-RAM-error/m-p/1020403#M150906</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-11-21T06:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulp RAM error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-RAM-error/m-p/1020404#M150907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;memtester errors description can be found on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.micromat.com/component/kunena/techtool-pro-7/4112-memory-test-failing-solid-bits" title="https://www.micromat.com/component/kunena/techtool-pro-7/4112-memory-test-failing-solid-bits"&gt;Micromat :: Topic: Memory test failing solid bits (1/1)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://unix.stackexchange.com/questions/439755/what-can-i-do-with-the-output-of-memtester-when-it-shows-bad-memory" title="https://unix.stackexchange.com/questions/439755/what-can-i-do-with-the-output-of-memtester-when-it-shows-bad-memory"&gt;ram - What can I do with the output of memtester when it shows bad memory? - Unix &amp;amp; Linux Stack Exchange&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For new memory it is necessary to run ddr test &lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V3.00&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and update ddr settings found from test in uboot&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7ulp_evk/imximage.cfg?h=imx_v2018.03_4.14.98_2.2.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7ulp_evk/imximage.cfg?h=imx_v2018.03_4.14.98_2.2.0"&gt;imximage.cfg\mx7ulp_evk\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 07:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulp-RAM-error/m-p/1020404#M150907</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-11-21T07:30:15Z</dc:date>
    </item>
  </channel>
</rss>