<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MM EVK DDR4 eMMC error while using uuu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020188#M150868</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/raajeshk88@gmail.com"&gt;raajeshk88@gmail.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems i.MX8M Mini EVK with DDR4 has NAND flash instead of eMMC. For your reference, I have attached the SOM board schematic file, you need to use u-boot file for&amp;nbsp;NAND or SD card in case of DDR4 EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feel free to let us know if you still face any issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 May 2020 10:00:50 GMT</pubDate>
    <dc:creator>kunalkotecha1</dc:creator>
    <dc:date>2020-05-04T10:00:50Z</dc:date>
    <item>
      <title>IMX8MM EVK DDR4 eMMC error while using uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020187#M150867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using im8mm EVK with DDR4. while to flash the images from NXP&amp;nbsp;L4.14.98_2.0.0_ga_images_MX8MMEVK.zip .&lt;/P&gt;&lt;P&gt;uuu.exe -b emmc_all imx-boot-imx8mmddr4evk-sd.bin-flash_ddr4_evk fsl-image-validation-imx-imx8mmevk.sdcard or&lt;/P&gt;&lt;P&gt;uuu.exe -b emmc_all imx-boot-imx8mmddr4evk-sd.bin-flash_ddr4_evk fsl-image-validation-imx-imx8mmevk.tar.bz2\*&lt;/P&gt;&lt;P&gt;I am getting this error&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2:5 3/ 8 [ ] FB: ucmd mmc dev ${emmc_dev}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;meanwhile in the serial port we are getting this&lt;/P&gt;&lt;P&gt;U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 13:37:29 +0000)&lt;BR /&gt;power_bd71837_init&lt;BR /&gt;DRAM PHY training for 2400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;DRAM PHY training for 400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;DRAM PHY training for 100MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;DRAM PHY training for 2400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from USB SDP&lt;BR /&gt;SDP: initialize...&lt;BR /&gt;SDP: handle requests...&lt;BR /&gt;Downloading file of size 1451348 to 0x40400000... done&lt;BR /&gt;Jumping to header at 0x40400000&lt;BR /&gt;Header Tag is not an IMX image&lt;BR /&gt;Found header at 0x4042c200&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 13:37:29 +0000)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 44C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: FSL i.MX8MM DDR4 EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]&lt;BR /&gt;SNK.Power3.0 on CC1&lt;BR /&gt;tcpc_pd_receive_message: Polling ALERT register, TCPC_ALERT_RX_STATUS bit failed, ret = -62&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;NAND: 0 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from MMC... Card did not respond to voltage select!&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;No panel detected: default to MIPI2HDMI&lt;BR /&gt;adv7535_init: Can't find device id=0x3d, on bus 1&lt;BR /&gt;Display: MIPI2HDMI (1920x1080)&lt;BR /&gt;Video: 1920x1080x24&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt; - ATF 1cb68fa&lt;BR /&gt; - U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df&lt;/P&gt;&lt;P&gt;Card did not respond to voltage select!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Boot from USB for mfgtools&lt;BR /&gt;Use default environment for mfgtools&lt;BR /&gt;Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;/P&gt;&lt;P&gt;## Checking Image at 43800000 ...&lt;BR /&gt;Unknown image format!&lt;BR /&gt;Run fastboot ...&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:0&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;MMC card init failed!&lt;BR /&gt;Card did not respond to voltage select!&lt;BR /&gt;** Block device MMC 0 not supported&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;MMC Device 1 not found&lt;BR /&gt;invalid mmc device 1&lt;BR /&gt;MMC Device 1 not found&lt;BR /&gt;no mmc device at slot 1&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;Detect USB boot. Will enter fastboot mode!&lt;BR /&gt;MMC Device 1 not found&lt;BR /&gt;no mmc device at slot 1&lt;BR /&gt;&lt;BR /&gt;this seems to be an issue with HW. what im missing here.thanks&lt;BR /&gt;&lt;BR /&gt;could you also provide the datasheet for the iMX8MM EVK with DDR4. I see this board only has one MMC and no NAND . thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 06:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020187#M150867</guid>
      <dc:creator>raajeshk88</dc:creator>
      <dc:date>2020-02-27T06:25:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK DDR4 eMMC error while using uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020188#M150868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/raajeshk88@gmail.com"&gt;raajeshk88@gmail.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems i.MX8M Mini EVK with DDR4 has NAND flash instead of eMMC. For your reference, I have attached the SOM board schematic file, you need to use u-boot file for&amp;nbsp;NAND or SD card in case of DDR4 EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Feel free to let us know if you still face any issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2020 10:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020188#M150868</guid>
      <dc:creator>kunalkotecha1</dc:creator>
      <dc:date>2020-05-04T10:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK DDR4 eMMC error while using uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020189#M150869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Thanks for sharing the schematic. Yes its only NAND and SD card and we were successful in using the uuu. I would suggest to provide docs on all variation of EVK in the website. There is a difference of Wifi/BT module as well. Some uses Qualcomm 1PJ and some Cypress 1MW.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Raajesh K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2020 07:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020189#M150869</guid>
      <dc:creator>raajeshk88</dc:creator>
      <dc:date>2020-05-05T07:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK DDR4 eMMC error while using uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020190#M150870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/raajeshk88@gmail.com"&gt;raajeshk88@gmail.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download design files for both&amp;nbsp;revisions from the below link.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-mini-applications-processor:8MMINILPD4-EVK" title="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-mini-applications-processor:8MMINILPD4-EVK"&gt;i.MX 8M Mini Evaluation Kit | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2020 08:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-DDR4-eMMC-error-while-using-uuu/m-p/1020190#M150870</guid>
      <dc:creator>kunalkotecha1</dc:creator>
      <dc:date>2020-05-05T08:55:25Z</dc:date>
    </item>
  </channel>
</rss>