<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックflash SabreSD with uuu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/flash-SabreSD-with-uuu/m-p/1020138#M150859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Before bringing up a custom board, I'm trying to master the flashing process with an SabreSD board reworked for emmc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the command for doing that?. As per help, I assume&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu -b emmc_all &amp;lt;u-boot.imx&amp;gt; &amp;lt;image&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where I'm using the files created with Yocto (deploy/images)&lt;/P&gt;&lt;P&gt;u-boot is file u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;image is core-image-minimal-imx6sxsabresd-20190724082608.rootfs.sdcard.bz2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flashing process stops after completing first step (boot).&lt;/P&gt;&lt;P&gt;I'm missing something? I'm not using the correct files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OUTPUT:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.130-0-g247629e&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt; Pctl Chip Vid Pid BcdVersion&lt;BR /&gt; ==================================================&lt;BR /&gt; SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt; SDPS: MX28 0x15a2 0x004f&lt;BR /&gt; SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt; SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt; SDP: MX7D 0x15a2 0x0076&lt;BR /&gt; SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt; SDP: MX6D 0x15a2 0x0061&lt;BR /&gt; SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt; SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt; SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt; SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt; SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt; SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt; SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt; SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt; SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt; FBK: 0x066f 0x9afe&lt;BR /&gt; FBK: 0x066f 0x9bff&lt;BR /&gt; FB: 0x0525 0xa4a5&lt;BR /&gt; FB: 0x18d1 0x0d02&lt;/P&gt;&lt;P&gt;Run built-in script:&lt;BR /&gt; &lt;BR /&gt;uuu_version 1.2.39&lt;/P&gt;&lt;P&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash -raw2sparse all /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/core-image-minimal-imx6sxsabresd-20190724082608.rootfs.sdcard.bz2/*&lt;BR /&gt;FB: flash bootloader /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: done&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 2:34&lt;BR /&gt;2:34&amp;gt;Start Cmd:SDP: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;BR /&gt;6400%2:34&amp;gt;Okay (0.342s)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2020 11:36:43 GMT</pubDate>
    <dc:creator>V_Palacio</dc:creator>
    <dc:date>2020-02-26T11:36:43Z</dc:date>
    <item>
      <title>flash SabreSD with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flash-SabreSD-with-uuu/m-p/1020138#M150859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Before bringing up a custom board, I'm trying to master the flashing process with an SabreSD board reworked for emmc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the command for doing that?. As per help, I assume&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu -b emmc_all &amp;lt;u-boot.imx&amp;gt; &amp;lt;image&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where I'm using the files created with Yocto (deploy/images)&lt;/P&gt;&lt;P&gt;u-boot is file u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;image is core-image-minimal-imx6sxsabresd-20190724082608.rootfs.sdcard.bz2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flashing process stops after completing first step (boot).&lt;/P&gt;&lt;P&gt;I'm missing something? I'm not using the correct files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OUTPUT:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.130-0-g247629e&lt;/P&gt;&lt;P&gt;Build in config:&lt;BR /&gt; Pctl Chip Vid Pid BcdVersion&lt;BR /&gt; ==================================================&lt;BR /&gt; SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt; SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt; SDPS: MX28 0x15a2 0x004f&lt;BR /&gt; SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt; SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt; SDP: MX7D 0x15a2 0x0076&lt;BR /&gt; SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt; SDP: MX6D 0x15a2 0x0061&lt;BR /&gt; SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt; SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt; SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt; SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt; SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt; SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt; SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt; SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt; SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt; SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt; SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt; FBK: 0x066f 0x9afe&lt;BR /&gt; FBK: 0x066f 0x9bff&lt;BR /&gt; FB: 0x0525 0xa4a5&lt;BR /&gt; FB: 0x18d1 0x0d02&lt;/P&gt;&lt;P&gt;Run built-in script:&lt;BR /&gt; &lt;BR /&gt;uuu_version 1.2.39&lt;/P&gt;&lt;P&gt;# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ&lt;BR /&gt;SDP: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;# This command will be run when ROM support stream mode&lt;BR /&gt;# i.MX8QXP, i.MX8QM&lt;BR /&gt;SDPS: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# SDPU will be deprecated. please use SDPV instead of SDPU&lt;BR /&gt;# {&lt;BR /&gt;SDPU: delay 1000&lt;BR /&gt;SDPU: write -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx -offset 0x57c00&lt;BR /&gt;SDPU: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;# These commands will be run when use SPL and will be skipped if no spl&lt;BR /&gt;# if (SPL support SDPV)&lt;BR /&gt;# {&lt;BR /&gt;SDPV: delay 1000&lt;BR /&gt;SDPV: write -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx -skipspl&lt;BR /&gt;SDPV: jump&lt;BR /&gt;# }&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;FB: ucmd setenv fastboot_dev mmc&lt;BR /&gt;FB: ucmd setenv mmcdev ${emmc_dev}&lt;BR /&gt;FB: ucmd mmc dev ${emmc_dev}&lt;BR /&gt;FB: flash -raw2sparse all /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/core-image-minimal-imx6sxsabresd-20190724082608.rootfs.sdcard.bz2/*&lt;BR /&gt;FB: flash bootloader /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;BR /&gt;FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;&lt;BR /&gt;FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0&lt;BR /&gt;FB: done&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 2:34&lt;BR /&gt;2:34&amp;gt;Start Cmd:SDP: boot -f /bsp/imx-yocto-bsp-sabre/build/tmp/deploy/images/imx6sxsabresd/u-boot-imx6sxsabresd.imx&lt;BR /&gt;6400%2:34&amp;gt;Okay (0.342s)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 11:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flash-SabreSD-with-uuu/m-p/1020138#M150859</guid>
      <dc:creator>V_Palacio</dc:creator>
      <dc:date>2020-02-26T11:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: flash SabreSD with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/flash-SabreSD-with-uuu/m-p/1020139#M150860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;What is the command for doing that?. As per help, I assume&amp;nbsp;&lt;/P&gt;&lt;P&gt;uuu -b emmc_all &amp;lt;u-boot.imx&amp;gt; &amp;lt;image&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;gt; Yes you're correct&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Flashing process stops after completing first step (boot).&lt;/P&gt;&lt;P&gt;I'm missing something? I'm not using the correct files?&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;gt; I believe that you may be using an old uboot version, by default it is not supported since UUU needs to have fastboot enabled in uboot, please note that if using an older BSP (equal or lower than L4.9.88_2.0.0) you may use old MFGTool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I see that you want to test the tool, you may download any of the Linux BSP (L4.14.78_1.0.0 or higher) we have available here:&lt;BR /&gt; &lt;A href="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW"&gt;https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tools:IMX-SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Aldo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 17:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/flash-SabreSD-with-uuu/m-p/1020139#M150860</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2020-03-09T17:58:17Z</dc:date>
    </item>
  </channel>
</rss>