<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can I use opencv for imx6?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020133#M150856</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can download L4.14.98_2.0.0_MX6QDLSOLOX BSP here:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;BR /&gt;it has OpenCV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Feb 2020 04:51:58 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-02-13T04:51:58Z</dc:date>
    <item>
      <title>Can I use opencv for imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020132#M150855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I use opencv for imx6?&lt;/P&gt;&lt;P&gt;When I use the gst-launch command。&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;gst-launch 1.0 imxv4l2src device=/dev/video0! Imxv4l2sink device = / dev/video16&lt;/P&gt;&lt;P&gt;&amp;nbsp; /dev/video0 mean ov5640&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;/dev/video16 mean display device&lt;/P&gt;&lt;P&gt;It can display the image of the camera on the display device。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when i use opencv,error&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;VIDEOIO ERROR: libv4l unable to ioctl S_FMT&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;VIDEOIO ERROR: libv4l unable to ioctl VIDIOCSPICT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;source :&lt;BR /&gt;#include &amp;lt;opencv2/ opencv.hpp&amp;gt;&lt;BR /&gt;#include &amp;lt;opencv2/imgproc.hpp&amp;gt;&lt;BR /&gt;#include &amp;lt;opencv2/highgui. hpp&amp;gt;&lt;BR /&gt;#include &amp;lt;opencv2/videoio. hpp&amp;gt;&lt;BR /&gt;#include &amp;lt;iostream&amp;gt;&lt;BR /&gt;using nanespace CV;&lt;BR /&gt;using namespace std;&lt;BR /&gt;int main()&lt;BR /&gt;{&lt;BR /&gt;cout&amp;lt;&amp;lt;"Built with opencv"&amp;lt;&amp;lt;CV_ VERSION&amp;lt;&amp;lt;endl;&lt;BR /&gt;VideoCapture capture(0);&lt;BR /&gt;if( !capture. isopened())&lt;BR /&gt;cout&amp;lt;&amp;lt;"open camera failed."&amp;lt;&amp;lt;endl;&lt;BR /&gt;return - 1;&lt;BR /&gt;}&lt;BR /&gt;Mat frame;&lt;BR /&gt;while( 1)&lt;BR /&gt;capture&amp;gt;&amp;gt;frame ;&lt;BR /&gt;if(frame . empty())&lt;BR /&gt;break;&lt;BR /&gt;imshow( "video" , frame);&lt;BR /&gt;if(waitKey(20)&amp;gt;0)&lt;BR /&gt;break;&lt;BR /&gt;}&lt;BR /&gt;return 0;&lt;/P&gt;&lt;P&gt;I didn't make any changes to the kernel，I just wrote a test program to test opencv。&lt;/P&gt;&lt;P&gt;Why the error？&lt;/P&gt;&lt;P&gt;Or how do I pass the data from gst-launch to opencv?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;VideoCapture capture(gst-launch .......“”);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;May I do that?&lt;/P&gt;&lt;P&gt;If so, what should be the order?&lt;/P&gt;&lt;P&gt;thank you！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 02:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020132#M150855</guid>
      <dc:creator>zhiyuan_song</dc:creator>
      <dc:date>2020-02-13T02:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use opencv for imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020133#M150856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can download L4.14.98_2.0.0_MX6QDLSOLOX BSP here:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i.mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;BR /&gt;it has OpenCV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 04:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020133#M150856</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-02-13T04:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use opencv for imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020134#M150857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've downloaded opencv, set up opencv's cross-compilation environment, and ported it to the imx6 development board.&lt;/P&gt;&lt;P&gt;This is not the reason for BSP, is it? Does imx6 support the use of opencv?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 05:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020134#M150857</guid>
      <dc:creator>zhiyuan_song</dc:creator>
      <dc:date>2020-02-13T05:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use opencv for imx6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020135#M150858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it does, if you are not going to use any hardware acceleration OpenCV, you can ran with no problem, but if you want something like OVX or OCL support, then you need to move to i.MX8.&amp;nbsp; You can check some info about opencv and imx6 at &lt;A href="http://www.imxcv.blogspot.com"&gt;www.imxcv.blogspot.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 06:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-use-opencv-for-imx6/m-p/1020135#M150858</guid>
      <dc:creator>andre_silva</dc:creator>
      <dc:date>2020-07-23T06:26:06Z</dc:date>
    </item>
  </channel>
</rss>