<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Enabling boot console in Yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020110#M150851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you tell me which BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Nov 2019 08:28:18 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2019-11-08T08:28:18Z</dc:date>
    <item>
      <title>Enabling boot console in Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020109#M150850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project using an iMX6 and Yocto with kernel version 4.1.15. I would like to get a verbose output from the kernel sent to the serial console during the boot process. I have passed earlyprintk as a parameter to the kernel from uboot, and when the system boot I get the following output in the console:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Starting kernel ...&lt;BR /&gt;&lt;BR /&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Booting Linux on physical CPU 0x0&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Linux version 4.1.15-yocto-standard (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #5 SMP PREEMPT Wed Nov 6 18:31:45 CE&lt;BR /&gt;T 2019&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Machine model: MSC Q7 i.MX6Q (143)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] bootconsole [earlycon0] enabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory policy: Data cache writealloc&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] PERCPU: Embedded 12 pages/cpu @ee7a0000 s17100 r8192 d23860 u49152&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 520720&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Kernel command line:&amp;nbsp; coherent_pool=16M earlyprintk earlycon=imx21-uart,0x21e8000,115200n8 ttymxc1,115200 consoleblan&lt;BR /&gt;k=0 mtdparts=m25p16:0x0000020000@0x0000000000(init),0x0000020000@0x0000020000(uboot_data),0x0000080000@0x0000040000(uboot),0x0000140&lt;BR /&gt;000@0x00000c0000(boot_logo) root=/dev/mmcblk0p1 rw,rootwait ip=:::::eth0:off fec.macaddr=0x00,0x30,0xD6,0x16,0x48,0x85&amp;nbsp;&amp;nbsp;&amp;nbsp; board_name&lt;BR /&gt;=msc-q7-imx6plus board_id=1004305806 board_variant=143-012 boot_count=1211&amp;nbsp;&amp;nbsp;&amp;nbsp; uboot_version=2014.04+g3a5fc25&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory: 1739116K/2097152K available (8147K kernel code, 369K rwdata, 2644K rodata, 316K init, 498K bss, 358036K reser&lt;BR /&gt;ved, 0K cma-reserved, 270336K highmem)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Virtual kernel memory layout:&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vector&amp;nbsp; : 0xffff0000 - 0xffff1000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 4 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fixmap&amp;nbsp; : 0xffc00000 - 0xfff00000&amp;nbsp;&amp;nbsp; (3072 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vmalloc : 0xf0000000 - 0xff000000&amp;nbsp;&amp;nbsp; ( 240 MB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lowmem&amp;nbsp; : 0x80000000 - 0xef800000&amp;nbsp;&amp;nbsp; (1784 MB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pkmap&amp;nbsp;&amp;nbsp; : 0x7fe00000 - 0x80000000&amp;nbsp;&amp;nbsp; (&amp;nbsp;&amp;nbsp; 2 MB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; modules : 0x7f000000 - 0x7fe00000&amp;nbsp;&amp;nbsp; (&amp;nbsp; 14 MB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .text : 0x80008000 - 0x80a9206c&amp;nbsp;&amp;nbsp; (10793 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .init : 0x80a93000 - 0x80ae2000&amp;nbsp;&amp;nbsp; ( 316 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x80ae2000 - 0x80b3e440&amp;nbsp;&amp;nbsp; ( 370 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .bss : 0x80b3e440 - 0x80bbaf10&amp;nbsp;&amp;nbsp; ( 499 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Preemptible hierarchical RCU implementation.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] NR_IRQS:16 nr_irqs:16 16&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 erratum 769419 enabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 enabling early BRESP for Cortex-A9&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 full line of zeros enabled for Cortex-A9&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 ID prefetch enabled, offset 16 lines&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] ccm: ldb_di_sel already changed from reset value&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] mxc_clocksource_init 3000000&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Switching to timer-based delay loop, resolution 333ns&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000009] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.008300] clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.018922] Console: colour dummy device 80x30&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.023479] console [tty0] enabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.026986] bootconsole [earlycon0] disabled&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;After the line stating the bootconsole is disabled, I see no further output until the login prompt.I have spent some time searching for an answer, but so far I've not found anything that helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I enable the boot console so I get a verbose output from the kernel during booting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6 quadplus‌&lt;/P&gt;&lt;P&gt;yocto warrior‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 15:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020109#M150850</guid>
      <dc:creator>ajellisuk</dc:creator>
      <dc:date>2019-11-07T15:50:34Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling boot console in Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020110#M150851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you tell me which BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 08:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020110#M150851</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-11-08T08:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling boot console in Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020111#M150852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmy&lt;/P&gt;&lt;P&gt;Thank you for your reply&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BSP I'm using is for msc-q7-imx6plus (&lt;SPAN lang="EN-US" style="font-size: 11pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;MSC-LDK v1.3.0&lt;/SPAN&gt;) :&lt;BR /&gt;&lt;A class="link-titled" href="https://www.msc-technologies.eu/products-solutions/products/boards/qseven/msc-q7-imx6plus.html" title="https://www.msc-technologies.eu/products-solutions/products/boards/qseven/msc-q7-imx6plus.html"&gt;MSC Q7-IMX6PLUS: MSC technologies an Avnet Company&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Nov 2019 09:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020111#M150852</guid>
      <dc:creator>ajellisuk</dc:creator>
      <dc:date>2019-11-08T09:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling boot console in Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020112#M150853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the log message "bootconsole [earlycon0] disabled", the bootconsole was disabled. There somewhere disable the earlycon may due to conflict with the usage of the same uart port or debug port. May be in driver or board .c file in the BSP. If you cannot find it from the BSP source code, it is better to check with the provider/company of the BSP.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Nov 2019 07:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020112#M150853</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-11-11T07:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling boot console in Yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020113#M150854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jimmy&lt;/P&gt;&lt;P&gt;After further searching&amp;nbsp; I found‌ the answer:&lt;/P&gt;&lt;P&gt;There was an environment variable in uboot which read, "console=ttymxc1,115200", it needed to be changed so that it reads, "console=console=ttymxc1,115200".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I now get all of the messages from the kernel I need during boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 11:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-boot-console-in-Yocto/m-p/1020113#M150854</guid>
      <dc:creator>ajellisuk</dc:creator>
      <dc:date>2019-11-12T11:06:28Z</dc:date>
    </item>
  </channel>
</rss>