<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIPI Display to IMX8 MQ</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019965#M150830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is correct, the DCSS&amp;nbsp; is the module that generates the configuration parameters of the MIPI DSI BRIDGE so your path &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dcss -&amp;gt; mipi_dsi -&amp;gt; mipi_dsi_bridge &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2020 15:15:42 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2020-02-26T15:15:42Z</dc:date>
    <item>
      <title>MIPI Display to IMX8 MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019964#M150829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;We have connected MIPI display to imx8 MQ, We are concern like panel information along with display-timing parameter shall be defined in in dts file. whether panel and display parameter shall be defined in mipi_dsi node or mipi_dsi_bridge node.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MIPI display runs on frequency 77.94 MHZ, Is it possible to provide the clock in the Kernel version (4.14.98-gb6ce727-dirty)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we connect MIPI display to imx8 MQ via MIPI interface what is need to mipi_dsi_bridge node?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dcss -&amp;gt; mipi_dsi -&amp;gt; mipi_dsi_bridge (define display-timings parameter)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kishore P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 12:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019964#M150829</guid>
      <dc:creator>kishorepoojari</dc:creator>
      <dc:date>2020-02-26T12:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI Display to IMX8 MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019965#M150830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is correct, the DCSS&amp;nbsp; is the module that generates the configuration parameters of the MIPI DSI BRIDGE so your path &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dcss -&amp;gt; mipi_dsi -&amp;gt; mipi_dsi_bridge &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 15:15:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019965#M150830</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2020-02-26T15:15:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI Display to IMX8 MQ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019966#M150831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jamesbone,&lt;/P&gt;&lt;P&gt;Thanks for the information, We have 2 problem (Kernel Version :4.14.98) ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Our custom display works at the clock rate 77.94 MHZ, But we are unable to set the clock at the required frequency. If&amp;nbsp; we set the clock at 77.94 MHZ we are getting below Error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.784154] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.791665] nwl_dsi-imx mipi_dsi@30A00000: Using DCSS as input source&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.798870] nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x415&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.808957] imx-drm display-subsystem: bound mipi_dsi@30A00000 (ops imx_nwl_dsi_component_ops)&lt;BR /&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.817634] [drm] Cannot find any crtc or sizes&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. If we set the Clock at 80 MHZ command are sent via MIPI interface (Display is not responding right now), We are getting below error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.820041] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.827551] nwl_dsi-imx mipi_dsi@30A00000: Using DCSS as input source&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.834752] nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x415&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 1.844818] imx-drm display-subsystem: bound mipi_dsi@30A00000 (ops imx_nwl_dsi_component_ops)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.615899] panel-auo-ili2117a 30a00000.mipi_dsi_bridge.0: [drm:rad_panel_enable] *&lt;STRONG&gt;ERROR&lt;/STRONG&gt;*&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.615899]&amp;nbsp; Send MCS success&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.655974] Console: switching to colour frame buffer device 90x80&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.708295] imx-drm display-subsystem: fb0:&amp;nbsp; frame buffer device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help us to solve the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kishore P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 05:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-Display-to-IMX8-MQ/m-p/1019966#M150831</guid>
      <dc:creator>kishorepoojari</dc:creator>
      <dc:date>2020-02-27T05:11:57Z</dc:date>
    </item>
  </channel>
</rss>