<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Problem on touchscreen on IMX53-START-R board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222757#M15073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've a IMX53-START-R board connected ti a MCIMX-LVDS1 board.&lt;/P&gt;&lt;P&gt;The software I'm using is the one provided on the original SD card (the name I think is UBUNTU 11_09 DEMO IMAGE).&lt;/P&gt;&lt;P&gt;I think I've properly configurated the boot (setting the bootargs_base parameter) in order to use a LVDS display; in fact, I see the ubuntu 10.04 desktop and I can use usb mouse and keyboard properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I can't use is the touchscreen. If I use the "virgin" SD card, if I touch the screen I see the mouse cursor go to the center of the screen. The procedure for configure the touchscreen doesn't work and seems to be sensible to the mouse pointer and not to the touchscreen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to look to the older post and I've seen a problem similar to mine:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/302173"&gt;imx53qsb with ubuntu 10.04 and MCIMX-LVDS1 touchscreen&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try that procedure but, when I touch the screen, the cursor goes to the upper left corner. What am I doing wrong?&lt;/P&gt;&lt;P&gt;I think the touch screen is "captured" by the system but not properly. Is there something I can do in order to use the touchscreen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Mar 2013 09:03:41 GMT</pubDate>
    <dc:creator>stefanobizzari</dc:creator>
    <dc:date>2013-03-13T09:03:41Z</dc:date>
    <item>
      <title>Problem on touchscreen on IMX53-START-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222757#M15073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've a IMX53-START-R board connected ti a MCIMX-LVDS1 board.&lt;/P&gt;&lt;P&gt;The software I'm using is the one provided on the original SD card (the name I think is UBUNTU 11_09 DEMO IMAGE).&lt;/P&gt;&lt;P&gt;I think I've properly configurated the boot (setting the bootargs_base parameter) in order to use a LVDS display; in fact, I see the ubuntu 10.04 desktop and I can use usb mouse and keyboard properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I can't use is the touchscreen. If I use the "virgin" SD card, if I touch the screen I see the mouse cursor go to the center of the screen. The procedure for configure the touchscreen doesn't work and seems to be sensible to the mouse pointer and not to the touchscreen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to look to the older post and I've seen a problem similar to mine:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/302173"&gt;imx53qsb with ubuntu 10.04 and MCIMX-LVDS1 touchscreen&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try that procedure but, when I touch the screen, the cursor goes to the upper left corner. What am I doing wrong?&lt;/P&gt;&lt;P&gt;I think the touch screen is "captured" by the system but not properly. Is there something I can do in order to use the touchscreen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2013 09:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222757#M15073</guid>
      <dc:creator>stefanobizzari</dc:creator>
      <dc:date>2013-03-13T09:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on touchscreen on IMX53-START-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222758#M15074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG style="font-size: 12px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&lt;A href="https://community.nxp.com/people/stefanobizzari"&gt;stefanobizzari&lt;/A&gt;&lt;/STRONG&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried calibrating the touch screen ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards,&lt;/P&gt;&lt;P&gt;Keshava G N&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 07:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222758#M15074</guid>
      <dc:creator>KeshavaGN</dc:creator>
      <dc:date>2013-03-14T07:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on touchscreen on IMX53-START-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222759#M15075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, as I said, the calibration doesn't work and the calibration is "sensible" to the mouse and not to the touch screen..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've seen that I can read the value of the touch screen on event2. In fact, if I try "sudo evtest /dev/input/event2" I see the X Y values and datas from the touchscreen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you got any idea for make my touchpanel work?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 08:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222759#M15075</guid>
      <dc:creator>stefanobizzari</dc:creator>
      <dc:date>2013-03-14T08:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on touchscreen on IMX53-START-R board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222760#M15076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following may help :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1463"&gt;I.MX53 Qt LVDS display&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 08:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-on-touchscreen-on-IMX53-START-R-board/m-p/222760#M15076</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-03-14T08:45:48Z</dc:date>
    </item>
  </channel>
</rss>