<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8QM EVK doesn't boot on SD card in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-EVK-doesn-t-boot-on-SD-card/m-p/1018186#M150619</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So far I have not been able to successfully get the i.MX 8QuadMax MEK board to boot.&amp;nbsp; Ideally, I would like to get this eval kit booting and to flash the M4 binary, with Trace32, however, I cannot seem to get the provided Linux image to boot from the SD card, either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initially I tried writing a SCFW image (provided by Lauterbach) to the SD card.&amp;nbsp; After doing this I attempted to load an M4 binary using Trace32, however T32 reported that there were CPU Bus errors when attempting to attach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point, I assumed that there could be issues with the SCFW image and decided to try simply using the IMX8QM Linux image, which is provided at the "IMXPRERELEASES: Alpha / Beta BSPs for Microprocessors" page: &lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license" title="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license"&gt;https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license &lt;/A&gt;.&amp;nbsp; This was not successful either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steps taken:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Writing SCFW or Linux image to SD card&lt;/LI&gt;&lt;LI&gt;Inserting SD card into J19&lt;/LI&gt;&lt;LI&gt;Setting the Boot Switch Selection (SW2) with POS-3 and POS-4 ON for Boot Device SD1, with the rest of the switches in the OFF position.&lt;/LI&gt;&lt;LI&gt;With the SCFW image:&lt;OL style="list-style-type: lower-alpha;"&gt;&lt;LI&gt;Power Cyclic the board and attempting to flash the M4 software using T32.&lt;/LI&gt;&lt;LI&gt;Pressing the MEK Reset Button (SW3) and attempting to flash the M4 software using T32.&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;With the Linux L4.19.35_1.0.0_MX8QM image:&lt;OL style="list-style-type: lower-alpha;"&gt;&lt;LI&gt;Connecting the USB Debug port (J19)&lt;/LI&gt;&lt;LI&gt;Opening 2 PuTTY sessions (One for each FTDI connection that appears after connecting USB calbe ) with Baud rate: 115200 (as per the instructions in IMX8QUADMAXQSG.pdf).&lt;/LI&gt;&lt;LI&gt;Power Cycling or pressing the SW3&lt;/LI&gt;&lt;LI&gt;Hitting enter in both PuTTY terminals.&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the Linux case, are there any steps that I am missing in order for this board to successfully boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jan 2020 20:14:55 GMT</pubDate>
    <dc:creator>joshua_achinger</dc:creator>
    <dc:date>2020-01-29T20:14:55Z</dc:date>
    <item>
      <title>iMX8QM EVK doesn't boot on SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-EVK-doesn-t-boot-on-SD-card/m-p/1018186#M150619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So far I have not been able to successfully get the i.MX 8QuadMax MEK board to boot.&amp;nbsp; Ideally, I would like to get this eval kit booting and to flash the M4 binary, with Trace32, however, I cannot seem to get the provided Linux image to boot from the SD card, either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initially I tried writing a SCFW image (provided by Lauterbach) to the SD card.&amp;nbsp; After doing this I attempted to load an M4 binary using Trace32, however T32 reported that there were CPU Bus errors when attempting to attach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point, I assumed that there could be issues with the SCFW image and decided to try simply using the IMX8QM Linux image, which is provided at the "IMXPRERELEASES: Alpha / Beta BSPs for Microprocessors" page: &lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license" title="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license"&gt;https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_MX8QM&amp;amp;appType=license &lt;/A&gt;.&amp;nbsp; This was not successful either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Steps taken:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Writing SCFW or Linux image to SD card&lt;/LI&gt;&lt;LI&gt;Inserting SD card into J19&lt;/LI&gt;&lt;LI&gt;Setting the Boot Switch Selection (SW2) with POS-3 and POS-4 ON for Boot Device SD1, with the rest of the switches in the OFF position.&lt;/LI&gt;&lt;LI&gt;With the SCFW image:&lt;OL style="list-style-type: lower-alpha;"&gt;&lt;LI&gt;Power Cyclic the board and attempting to flash the M4 software using T32.&lt;/LI&gt;&lt;LI&gt;Pressing the MEK Reset Button (SW3) and attempting to flash the M4 software using T32.&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;With the Linux L4.19.35_1.0.0_MX8QM image:&lt;OL style="list-style-type: lower-alpha;"&gt;&lt;LI&gt;Connecting the USB Debug port (J19)&lt;/LI&gt;&lt;LI&gt;Opening 2 PuTTY sessions (One for each FTDI connection that appears after connecting USB calbe ) with Baud rate: 115200 (as per the instructions in IMX8QUADMAXQSG.pdf).&lt;/LI&gt;&lt;LI&gt;Power Cycling or pressing the SW3&lt;/LI&gt;&lt;LI&gt;Hitting enter in both PuTTY terminals.&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the Linux case, are there any steps that I am missing in order for this board to successfully boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 20:14:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-EVK-doesn-t-boot-on-SD-card/m-p/1018186#M150619</guid>
      <dc:creator>joshua_achinger</dc:creator>
      <dc:date>2020-01-29T20:14:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM EVK doesn't boot on SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-EVK-doesn-t-boot-on-SD-card/m-p/1018187#M150620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Josh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for writing image &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_MX8QM&amp;amp;appType=license" target="_blank"&gt;Linux Biary Demo Files - i.MX 8QMax MEK&lt;/A&gt;&amp;nbsp; one can follow&lt;/P&gt;&lt;P&gt;sect.4.3.2 Copying the full SD card image attached Linux Guide or uuu tool.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools/" title="https://github.com/NXPmicro/mfgtools/"&gt;GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Full documentation can be found in &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS" target="_blank"&gt;Linux 4.19.35_1.1.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For M4 one can follow sect.7.3 Run an example application document&lt;/P&gt;&lt;P&gt;Getting Started with MCUXpresso SDK for i.MX 8QuadMax included in&lt;/P&gt;&lt;P&gt;SDK_MEK-MIMX8QM which can be obtained on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below short overview of boot process&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343178"&gt;i.MX8 Boot process and creating a bootable image&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Video :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-8quadmax-multisensory-enablement-kit-mek:MCIMX8QM-CPU" title="https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-8quadmax-multisensory-enablement-kit-mek:MCIMX8QM-CPU"&gt;i.MX 8QuadMax/QuadPlus Multisensory Enablement Kit | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 00:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-EVK-doesn-t-boot-on-SD-card/m-p/1018187#M150620</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-30T00:32:49Z</dc:date>
    </item>
  </channel>
</rss>