<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmfgtool error, device disconnect</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-error-device-disconnect/m-p/1017375#M150485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello forum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have to use mfgtools to burn a custom kernel,u-boot and rootfs into the board's NAND and the process can't complete because the tool keeps disconnecting the device. It doesn't report failure, but after it loads the initramfs, it starts booting from NAND after "Jumping to OS image". If we burn the vendor's image(no kernel modifications of our own), it works well, we have succeded in replacing the rootfs. If anyone can suggest a way forward?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mfgtools 2.7&lt;BR /&gt;Yocto 2.1&lt;BR /&gt;kernel 4.1.15&lt;BR /&gt;u-boot 2016.03&lt;BR /&gt;board: Myirtech's&amp;nbsp; MYS-6ULX-IOT (nxp's imx.6ull processor)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Nov 2019 20:00:24 GMT</pubDate>
    <dc:creator>sdi1100002</dc:creator>
    <dc:date>2019-11-06T20:00:24Z</dc:date>
    <item>
      <title>mfgtool error, device disconnect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-error-device-disconnect/m-p/1017375#M150485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello forum,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have to use mfgtools to burn a custom kernel,u-boot and rootfs into the board's NAND and the process can't complete because the tool keeps disconnecting the device. It doesn't report failure, but after it loads the initramfs, it starts booting from NAND after "Jumping to OS image". If we burn the vendor's image(no kernel modifications of our own), it works well, we have succeded in replacing the rootfs. If anyone can suggest a way forward?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mfgtools 2.7&lt;BR /&gt;Yocto 2.1&lt;BR /&gt;kernel 4.1.15&lt;BR /&gt;u-boot 2016.03&lt;BR /&gt;board: Myirtech's&amp;nbsp; MYS-6ULX-IOT (nxp's imx.6ull processor)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2019 20:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-error-device-disconnect/m-p/1017375#M150485</guid>
      <dc:creator>sdi1100002</dc:creator>
      <dc:date>2019-11-06T20:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool error, device disconnect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-error-device-disconnect/m-p/1017376#M150486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Katerina&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for custom board one can try to run ddr test and update Mfg Tool firmware &lt;BR /&gt;image with new ddr calibration coefficients found from test &lt;BR /&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;i.MX6/7 DDR Stress Test Tool V3.00&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;Update coefficients (example is for i.MX6Q Sabre SD board) in uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg&lt;/P&gt;&lt;P&gt;and then rebuild Mfg Tool firmware (files in&amp;nbsp; ../firmware folder, fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.&lt;/P&gt;&lt;P&gt;u-boot). For rebuilding use sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 00:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-error-device-disconnect/m-p/1017376#M150486</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-11-07T00:29:04Z</dc:date>
    </item>
  </channel>
</rss>