<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx6 disabled screen as console</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-disabled-screen-as-console/m-p/1016928#M150422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;BR /&gt;&amp;nbsp; My development board is IMX6Q-sabresd, and the version of my linux operating system is: 3.14.52.&lt;BR /&gt;Now I want to use my debug serial port as a normal serial port to transfer data. I changed console = ttymxc0 to console = error under uboot. With this modification, the debug serial port can be used as a normal serial port to communicate. But at startup, the init process will print some information to my lvds screen. This makes customers look uncomfortable.&lt;BR /&gt;Later I modified the configuration options of the kernel:&lt;BR /&gt;Configuration before modification:&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE = y&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY = y&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE_ROTATION = y&lt;/P&gt;&lt;P&gt;Modified configuration:&lt;BR /&gt;# CONFIG_FRAMEBUFFER_CONSOLE is not set&lt;/P&gt;&lt;P&gt;After the modification, the init process does not print information to my lvds screen, but my logo is not displayed on the screen when I boot up.&lt;/P&gt;&lt;P&gt;Is there any good solution to my current problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Mar 2020 09:18:09 GMT</pubDate>
    <dc:creator>864535720</dc:creator>
    <dc:date>2020-03-11T09:18:09Z</dc:date>
    <item>
      <title>imx6 disabled screen as console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-disabled-screen-as-console/m-p/1016928#M150422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;BR /&gt;&amp;nbsp; My development board is IMX6Q-sabresd, and the version of my linux operating system is: 3.14.52.&lt;BR /&gt;Now I want to use my debug serial port as a normal serial port to transfer data. I changed console = ttymxc0 to console = error under uboot. With this modification, the debug serial port can be used as a normal serial port to communicate. But at startup, the init process will print some information to my lvds screen. This makes customers look uncomfortable.&lt;BR /&gt;Later I modified the configuration options of the kernel:&lt;BR /&gt;Configuration before modification:&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE = y&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY = y&lt;BR /&gt;CONFIG_FRAMEBUFFER_CONSOLE_ROTATION = y&lt;/P&gt;&lt;P&gt;Modified configuration:&lt;BR /&gt;# CONFIG_FRAMEBUFFER_CONSOLE is not set&lt;/P&gt;&lt;P&gt;After the modification, the init process does not print information to my lvds screen, but my logo is not displayed on the screen when I boot up.&lt;/P&gt;&lt;P&gt;Is there any good solution to my current problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 09:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-disabled-screen-as-console/m-p/1016928#M150422</guid>
      <dc:creator>864535720</dc:creator>
      <dc:date>2020-03-11T09:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 disabled screen as console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-disabled-screen-as-console/m-p/1016929#M150423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below nxp linux repository&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Flinux-imx%2Ftree%2F%3Fh%3Dimx_4.9.88_2.0.0_ga" rel="nofollow" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga&lt;/A&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Flinux-imx%2Ftree%2F%3Fh%3Dimx_3.14.52_1.1.0_ga" rel="nofollow" target="_blank"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;dts example with uart2&lt;/P&gt;&lt;P&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Flinux-imx%2Ftree%2Farch%2Farm%2Fboot%2Fdts%2Fimx6q-arm2.dts%3Fh%3Dimx_3.14.52_1.1.0_ga" rel="nofollow" target="_blank"&gt;imx6q-arm2.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the u-boot logo you can refer to the thread in our community: &lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="98109" data-objecttype="102" href="https://community.nxp.com/docs/DOC-98109"&gt;Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Hope this can help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 16:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-disabled-screen-as-console/m-p/1016929#M150423</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-03-11T16:07:48Z</dc:date>
    </item>
  </channel>
</rss>