<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Yocto Sumo NXP : vkmark_1.0.bb:do_configure error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Sumo-NXP-vkmark-1-0-bb-do-configure-error/m-p/1016915#M150420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are building a yocto rootfs for iMX8M with wayland desktop environment. We are using the below repo link for downloading sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="test_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We could able to build "core-image-minimal" successfully.But when we try to build "fsl-image-qt5-validation-imx", we are getting vkmark do_configure issue. Also log shows that meson version (0.44.1) is below the required version (&amp;gt;=0.45).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_configure&lt;BR /&gt;| The Meson build system&lt;BR /&gt;| Version: 0.44.1&lt;BR /&gt;| Source dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/git&lt;BR /&gt;| Build dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build&lt;BR /&gt;| Build type: cross build&lt;BR /&gt;| &lt;BR /&gt;| Meson encountered an error in file meson.build, line 1, column 0:&lt;BR /&gt;| Meson version is 0.44.1 but project requires &amp;gt;=0.45.&lt;BR /&gt;| &lt;BR /&gt;| A full log can be found at /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build/meson-logs/meson-log.txt&lt;BR /&gt;| Build started at 2019-12-06T05:07:12.871010&lt;BR /&gt;| Main binary: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/recipe-sysroot-native/usr/bin/python3-native/python3&lt;BR /&gt;| Python system: Linux&lt;BR /&gt;| The Meson build system&lt;BR /&gt;| Version: 0.44.1&lt;BR /&gt;| Source dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/git&lt;BR /&gt;| Build dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build&lt;BR /&gt;| Build type: cross build&lt;BR /&gt;| ERROR: meson failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_configure (log file is located at /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/temp/log.do_configure.92735)&lt;BR /&gt;ERROR: Task (/data/iMX8m/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-graphics/vulkan/vkmark_1.0.bb:do_configure) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2130 tasks of which 2123 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We did cleansstate for meson, vkmark and fsl-image-qt5-validation-imx and triggered a build again. But still facing the same issue.&lt;/P&gt;&lt;P&gt;Please help us to resolve the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Antony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Dec 2019 05:54:59 GMT</pubDate>
    <dc:creator>antonyabeepraka</dc:creator>
    <dc:date>2019-12-06T05:54:59Z</dc:date>
    <item>
      <title>Yocto Sumo NXP : vkmark_1.0.bb:do_configure error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Sumo-NXP-vkmark-1-0-bb-do-configure-error/m-p/1016915#M150420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are building a yocto rootfs for iMX8M with wayland desktop environment. We are using the below repo link for downloading sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="test_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We could able to build "core-image-minimal" successfully.But when we try to build "fsl-image-qt5-validation-imx", we are getting vkmark do_configure issue. Also log shows that meson version (0.44.1) is below the required version (&amp;gt;=0.45).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_configure&lt;BR /&gt;| The Meson build system&lt;BR /&gt;| Version: 0.44.1&lt;BR /&gt;| Source dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/git&lt;BR /&gt;| Build dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build&lt;BR /&gt;| Build type: cross build&lt;BR /&gt;| &lt;BR /&gt;| Meson encountered an error in file meson.build, line 1, column 0:&lt;BR /&gt;| Meson version is 0.44.1 but project requires &amp;gt;=0.45.&lt;BR /&gt;| &lt;BR /&gt;| A full log can be found at /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build/meson-logs/meson-log.txt&lt;BR /&gt;| Build started at 2019-12-06T05:07:12.871010&lt;BR /&gt;| Main binary: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/recipe-sysroot-native/usr/bin/python3-native/python3&lt;BR /&gt;| Python system: Linux&lt;BR /&gt;| The Meson build system&lt;BR /&gt;| Version: 0.44.1&lt;BR /&gt;| Source dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/git&lt;BR /&gt;| Build dir: /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/build&lt;BR /&gt;| Build type: cross build&lt;BR /&gt;| ERROR: meson failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_configure (log file is located at /data/iMX8m/build-imx8m/tmp/work/aarch64-poky-linux/vkmark/1.0-r0/temp/log.do_configure.92735)&lt;BR /&gt;ERROR: Task (/data/iMX8m/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-graphics/vulkan/vkmark_1.0.bb:do_configure) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2130 tasks of which 2123 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We did cleansstate for meson, vkmark and fsl-image-qt5-validation-imx and triggered a build again. But still facing the same issue.&lt;/P&gt;&lt;P&gt;Please help us to resolve the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Antony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 05:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Sumo-NXP-vkmark-1-0-bb-do-configure-error/m-p/1016915#M150420</guid>
      <dc:creator>antonyabeepraka</dc:creator>
      <dc:date>2019-12-06T05:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Sumo NXP : vkmark_1.0.bb:do_configure error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Sumo-NXP-vkmark-1-0-bb-do-configure-error/m-p/1016916#M150421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Antony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need meson at least 0.45v to run yocto, uninstall and reinstall meson.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2019 15:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Sumo-NXP-vkmark-1-0-bb-do-configure-error/m-p/1016916#M150421</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-12-06T15:45:44Z</dc:date>
    </item>
  </channel>
</rss>