<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How do I upload user space application to Saber Dev kit in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016468#M150389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes. It can be done from that running Linux. &lt;BR /&gt;However I am not sure that there is ssh server in default configuration.&lt;BR /&gt;So you need to "get" the files from the board itself not "put" them there from the outside.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Feb 2020 09:42:39 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-02-03T09:42:39Z</dc:date>
    <item>
      <title>How do I upload user space application to Saber Dev kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016465#M150386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! I want to create a user space application and run this on the Linux user space (A7) of the dev kit. How do I upload/copy the application to the dev kit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 01:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016465#M150386</guid>
      <dc:creator>rlumo</dc:creator>
      <dc:date>2020-01-29T01:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: How do I upload user space application to Saber Dev kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016466#M150387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can add the files directly into the filesystem you build. &lt;BR /&gt;It can be done with coping the files to mounded SD card or directly into filesystem image with the command like these:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# mkdir fs&lt;BR /&gt;# dd if=imx-image-full-imx7dsabresd.sdcard of=imx-image-full-imx7dsabresd.sdcard2 bs=1k skip=32768 count=1632083&lt;BR /&gt;1632083+0 records in&lt;BR /&gt;1632083+0 records out&lt;BR /&gt;1671252992 bytes (1.7 GB) copied, 251.435 s, 6.6 MB/s&lt;BR /&gt;# mount imx-image-full-imx7dsabresd.sdcard2 fs -o loop&lt;BR /&gt;# cp -r your_software fs&lt;BR /&gt;# umount fs&lt;BR /&gt;# dd if=imx-image-full-imx7dsabresd.sdcard2 of=imx-image-full-imx7dsabresd.sdcard bs=1k seek=32768 count=1632083&lt;BR /&gt;1632083+0 records in&lt;BR /&gt;1632083+0 records out&lt;BR /&gt;1671252992 bytes (1.7 GB) copied, 145.696 s, 11.5 MB/s&lt;BR /&gt;# &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 06:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016466#M150387</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-01-29T06:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: How do I upload user space application to Saber Dev kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016467#M150388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. I will give this a go. &lt;/P&gt;&lt;P&gt;Is there a simpler method though, if the DevKit is running Linux, can I just not FTP or SSH to the dev kit and copy the file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 18:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016467#M150388</guid>
      <dc:creator>rlumo</dc:creator>
      <dc:date>2020-01-29T18:53:14Z</dc:date>
    </item>
    <item>
      <title>Re: How do I upload user space application to Saber Dev kit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016468#M150389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes. It can be done from that running Linux. &lt;BR /&gt;However I am not sure that there is ssh server in default configuration.&lt;BR /&gt;So you need to "get" the files from the board itself not "put" them there from the outside.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Feb 2020 09:42:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-upload-user-space-application-to-Saber-Dev-kit/m-p/1016468#M150389</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-02-03T09:42:39Z</dc:date>
    </item>
  </channel>
</rss>