<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IM8QM socketCAN access on yocto linux?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015489#M150269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the answer. It seems that fsl-imx8qm-mek-m4.dts got renamed to fsl-imx8qm-mek-rpmsg.dts and in fact flexcan is &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-rpmsg.dtsi?h=imx_4.19.35_1.1.0#n95"&gt;disabled &lt;/A&gt;there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I don't understand is that CAN works with the old test image, but not the new one. How can I enable it again? Is this intentionally?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp; Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 07:18:10 GMT</pubDate>
    <dc:creator>georglutz</dc:creator>
    <dc:date>2020-01-16T07:18:10Z</dc:date>
    <item>
      <title>IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015486#M150266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to access the socket can interfaces with a BSP &amp;gt;= L4.14.98_2.0.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an IMX8QM MEK board. When I boot the included SD card I can see socket CAN interfaces as well as the enabled device tree nodes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;root@imx8qmmek:~# ifconfig -s -a
Iface&amp;nbsp;&amp;nbsp; MTU Met&amp;nbsp;&amp;nbsp; RX-OK RX-ERR RX-DRP RX-OVR&amp;nbsp;&amp;nbsp;&amp;nbsp; TX-OK TX-ERR TX-DRP TX-OVR Flg
can0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 O
can1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 O
can2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 O
eth0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1500 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 99&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 105&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 BMdRU
lo&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 65536 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 90&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 90&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 LRU
root@imx8qmmek:~# cat /sys/firmware/devicetree/base/can\@5a8d0000/compatible
fsl,imx8qm-flexcanfsl,imx6q-flexcan
root@imx8qmmek:~# cat /sys/firmware/devicetree/base/can\@5a8d0000/status
okay
root@imx8qmmek:~# cat /sys/firmware/devicetree/base/can\@5a8e0000/status
okay
root@imx8qmmek:~# cat /sys/firmware/devicetree/base/can\@5a8f0000/status
okay&lt;/PRE&gt;&lt;P&gt;But the BSP version is rather old:&lt;/P&gt;&lt;P&gt;root@imx8qmmek:~# cat /etc/version &lt;BR /&gt;20181016062726&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E.g. with the image fsl-image-validation-imx-imx8qmmek.sdcard from BSP version L4.14.98_2.0.0 (&lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8QM&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX8QM&amp;amp;appType=license&lt;/A&gt;) there is no socket CAN interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;root@imx8qmmek:~# ifconfig -s -a
Iface&amp;nbsp;&amp;nbsp; MTU Met&amp;nbsp;&amp;nbsp; RX-OK RX-ERR RX-DRP RX-OVR&amp;nbsp;&amp;nbsp;&amp;nbsp; TX-OK TX-ERR TX-DRP TX-OVR Flg
eth0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1500 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 254&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 239&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 BMdRU
lo&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 65536 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 170&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 170&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 LRU&lt;/PRE&gt;&lt;P&gt;In fact the flexcan interfaces are disabled in the device tree:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;$ cat /sys/firmware/devicetree/base/can\@5a8d0000/compatible
fsl,imx8qm-flexcanfsl,imx6q-flexcan
cat /sys/firmware/devicetree/base/can\@5a8d0000/status
disabled
$ cat /sys/firmware/devicetree/base/can\@5a8e0000/status
disabled
$ cat /sys/firmware/devicetree/base/can\@5a8f0000/status
disabled&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So how can I bring CAN back to the A cores?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;&amp;nbsp; Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 11:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015486#M150266</guid>
      <dc:creator>georglutz</dc:creator>
      <dc:date>2020-01-15T11:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015487#M150267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The same effect (no CAN devices / CAN devices disabled in devicetree) can be seen with the test image imx-image-full-imx8qmmek.sdcard from the latest BSP &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_MX8QM&amp;amp;appType=license"&gt;4.19.35_1.1.0&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 12:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015487#M150267</guid>
      <dc:creator>georglutz</dc:creator>
      <dc:date>2020-01-15T12:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015488#M150268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Georg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all flexcans are enabled in fsl-imx8qm-mek.dtsi but disabled in fsl-imx8qm-mek-m4.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek.dtsi?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek.dtsi?h=imx_4.19.35_1.1.0"&gt;fsl-imx8qm-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tests can be performed using unit tests: &lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/can/doc?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/can/doc?h=imx_4.19.35_1.1.0"&gt;doc\can\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 00:32:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015488#M150268</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-16T00:32:18Z</dc:date>
    </item>
    <item>
      <title>Re: IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015489#M150269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the answer. It seems that fsl-imx8qm-mek-m4.dts got renamed to fsl-imx8qm-mek-rpmsg.dts and in fact flexcan is &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-rpmsg.dtsi?h=imx_4.19.35_1.1.0#n95"&gt;disabled &lt;/A&gt;there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I don't understand is that CAN works with the old test image, but not the new one. How can I enable it again? Is this intentionally?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp; Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 07:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015489#M150269</guid>
      <dc:creator>georglutz</dc:creator>
      <dc:date>2020-01-16T07:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015490#M150270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Georg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can to reenable some in fsl-imx8qm-mek-m4.dts and generate new image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 08:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015490#M150270</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-16T08:07:06Z</dc:date>
    </item>
    <item>
      <title>Re: IM8QM socketCAN access on yocto linux?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015491#M150271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried, see the other &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-341641?commentID=73425#comment-73675"&gt;thread&lt;/A&gt; , but without success ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp; Georg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 07:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IM8QM-socketCAN-access-on-yocto-linux/m-p/1015491#M150271</guid>
      <dc:creator>georglutz</dc:creator>
      <dc:date>2020-01-31T07:24:38Z</dc:date>
    </item>
  </channel>
</rss>