<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: OpenGL GLX extension to be checked</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014479#M150166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sandeep,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might find different errors in that code because the freeglut is not installed correctly,&amp;nbsp; however the HDMI display is EXPORT DISPLAY:0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Nov 2019 16:18:43 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-11-06T16:18:43Z</dc:date>
    <item>
      <title>OpenGL GLX extension to be checked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014478#M150165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OpenGL GLX extension is not supporting for hdmi display connected on im8qxp....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I ahve written a sample code based on glut...and run as following&lt;/P&gt;&lt;P&gt;freeglut (./sample): OpenGL GLX extension not supported by display ':0.0'&lt;/P&gt;&lt;P&gt;$Display was set to 0.0 and multiple...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to change display enviroment for OpenGL GLX extension, that works for this board...Linux-4.14.87+?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2019 15:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014478#M150165</guid>
      <dc:creator>sandeep_rai</dc:creator>
      <dc:date>2019-11-06T15:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: OpenGL GLX extension to be checked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014479#M150166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sandeep,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might find different errors in that code because the freeglut is not installed correctly,&amp;nbsp; however the HDMI display is EXPORT DISPLAY:0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2019 16:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014479#M150166</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-11-06T16:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: OpenGL GLX extension to be checked</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014480#M150167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FreeGlut binary are by-default installed to /usr/lib/ as libglut.so.x, libgl.so.x, libglu.so.x {glut dependency} and was unavailable .h files for glu, gl, and glut as include&amp;lt;GL/gl.h&amp;gt;, and glu.h, and glut.h but I resolved this using copying those header file from its yocto seems in yocto it was not by default instlled. But, any way when I compile the sample code based on glut in .cpp, I faced no error, but on run time i found this error: OpenGL GLX extension not supported by display ':0'&amp;nbsp;&amp;nbsp;&amp;nbsp; [DISPLAY=:0]&lt;/P&gt;&lt;P&gt;It is related to OpenGL&amp;nbsp; GLX error, seems GLX is not supporting. Alternate method, I have also used pyopengl for same but it also omitting same error.&lt;/P&gt;&lt;P&gt;Is GLX support HDMI DISPLAY?&lt;/P&gt;&lt;P&gt;IS GLX require another dependency like mesa-util, but in our case there is no mesa on yocto build or no available on Library in board file system related mesa?&lt;/P&gt;&lt;P&gt;Problem is at run time so I think, is there any issue related configuration for display, same code is running in Ubuntu/other PC?&lt;/P&gt;&lt;P&gt;Can You provide some Porting guide related to GLUT for this board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2019 05:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenGL-GLX-extension-to-be-checked/m-p/1014480#M150167</guid>
      <dc:creator>sandeep_rai</dc:creator>
      <dc:date>2019-11-07T05:49:31Z</dc:date>
    </item>
  </channel>
</rss>