<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't find PMIC[Error] in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-Error/m-p/1014087#M150136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Akash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to increase time between power-ups up to 20-30sec. to check&lt;/P&gt;&lt;P&gt;if issue is caused due to power-up sequence does not start with fully discharged board.&lt;/P&gt;&lt;P&gt;Also check that there were no other powered cables or supplies were connected to board.&lt;/P&gt;&lt;P&gt;Sect.4.2.1 Power-Up Sequence &lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processors for Consumer Products&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;states : "Need to ensure that there is no back voltage (leakage) from any supply on the board .."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Nov 2019 23:22:13 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-11-20T23:22:13Z</dc:date>
    <item>
      <title>Can't find PMIC[Error]</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-Error/m-p/1014086#M150135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using i.MX6ULL based board having PMIC(PFUZE3001) in which I am continuously power cycling the board for every 10 seconds. An application of SNVS RTC-wakeup is used to power ON the board after every 10 seconds. This application works properly for a certain period of time but after a point of time, it gives an error and stops the working of the board.&lt;/P&gt;&lt;P&gt;From logs(attached in attachment segment) it is seen that &lt;STRONG&gt;"Can't find PMIC: PFUZE3001"&lt;/STRONG&gt;.&amp;nbsp; And says "Please RESET the board."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Que: What is going wrong? And How can I solve it?&amp;nbsp;pmic fusing‌pmic reset&amp;nbsp;&lt;A href="https://community.nxp.com/t5/tag/imx processor/tg-p"&gt;#imx processor&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 06:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-Error/m-p/1014086#M150135</guid>
      <dc:creator>akashnair316</dc:creator>
      <dc:date>2019-11-20T06:21:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can't find PMIC[Error]</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-Error/m-p/1014087#M150136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Akash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to increase time between power-ups up to 20-30sec. to check&lt;/P&gt;&lt;P&gt;if issue is caused due to power-up sequence does not start with fully discharged board.&lt;/P&gt;&lt;P&gt;Also check that there were no other powered cables or supplies were connected to board.&lt;/P&gt;&lt;P&gt;Sect.4.2.1 Power-Up Sequence &lt;A href="https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf" target="_blank"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processors for Consumer Products&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;states : "Need to ensure that there is no back voltage (leakage) from any supply on the board .."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 23:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-find-PMIC-Error/m-p/1014087#M150136</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-11-20T23:22:13Z</dc:date>
    </item>
  </channel>
</rss>