<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX SoloLite / SLL: eInk Compatibility, Firmware, EoL in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-SoloLite-SLL-eInk-Compatibility-Firmware-EoL/m-p/1013836#M150116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both i.MX6SL and i.MX6SLL processors have Electrophoretic Display Controller (EPDC) that supports displays up to 4096 x 4096 pixels.&lt;BR /&gt;You can refer to chapter 21 of i.MX6SL Reference Manual and chapter 19 of i.MX6SLL RM for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6SL was launched in Nov 2012 and has 10 year longevity.&lt;BR /&gt;i.MX6SLL was launched in Jun 2017, so it will be produced at least till 2032.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can refer i.MX 6SLL Power Consumption Measurement:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12001.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12001.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is nothing special to i.MXSLL in point of Ethernet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jan 2020 04:45:52 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-01-30T04:45:52Z</dc:date>
    <item>
      <title>i.MX SoloLite / SLL: eInk Compatibility, Firmware, EoL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-SoloLite-SLL-eInk-Compatibility-Firmware-EoL/m-p/1013835#M150115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am planning on using the i.MX 6 SoloLite for a navigation tablet that my team is designing. I have several questions:&lt;/P&gt;&lt;P&gt;- is the i.MX SoloLite compatible with both Carta 1.2 and Pearl?&lt;/P&gt;&lt;P&gt;- Does NXP provide the EPD firmware for any eInk panel (Carta 1.2 or Pearl)?&lt;/P&gt;&lt;P&gt;- Is there a scheduled End-of-Life for the 6 SoloLite?&lt;/P&gt;&lt;P&gt;- knowing that the tablet will not be using Ethernet, is there an advantage in considering the SLL (consumption?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erwan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 19:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-SoloLite-SLL-eInk-Compatibility-Firmware-EoL/m-p/1013835#M150115</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2020-01-29T19:51:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX SoloLite / SLL: eInk Compatibility, Firmware, EoL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-SoloLite-SLL-eInk-Compatibility-Firmware-EoL/m-p/1013836#M150116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both i.MX6SL and i.MX6SLL processors have Electrophoretic Display Controller (EPDC) that supports displays up to 4096 x 4096 pixels.&lt;BR /&gt;You can refer to chapter 21 of i.MX6SL Reference Manual and chapter 19 of i.MX6SLL RM for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX6SL was launched in Nov 2012 and has 10 year longevity.&lt;BR /&gt;i.MX6SLL was launched in Jun 2017, so it will be produced at least till 2032.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can refer i.MX 6SLL Power Consumption Measurement:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12001.pdf" target="test_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12001.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is nothing special to i.MXSLL in point of Ethernet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2020 04:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-SoloLite-SLL-eInk-Compatibility-Firmware-EoL/m-p/1013836#M150116</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-01-30T04:45:52Z</dc:date>
    </item>
  </channel>
</rss>