<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 VPU library source and firmware in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013825#M150108</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to&amp;nbsp;support VPU encoding/decoding on Windows Embedded Compact 2013 (Windows CE).&amp;nbsp;My&amp;nbsp;intention is to port linux code, but I have some problems finding the source code. I'm definitely not a linux build nor Yocto expert, so I'm a little lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The source code for the VPU library is not included in the linux source available on codeaurora - neither in linux-imx nor in linux-lib nor elsewhere I looked at. Furthermore, I need also the binary blob for the VPU firmware (vpu_fw_imx6q.bin and&amp;nbsp;vpu_fw_imx6d.bin), which again seems not to be part of the imx-linux distribution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After&amp;nbsp;much googling I ended up at repository.timesys.com/buildsources,&amp;nbsp;which looks (to me) to "the" repo currently used by the Yocto distributions. There I found the compressed packages for both the&amp;nbsp; VPU library source and the VPU firmare, respectively:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin" title="http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin&lt;/A&gt;&amp;nbsp;(latest available)&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin" title="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Still, I have some questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1] Is timesys the/an official repository I can safely download up-to-date&amp;nbsp;i.MX linux sources from?&lt;/P&gt;&lt;P&gt;[2] Are those two packages (library 5.4.38 and firmware 5.4) compatible to each other?&lt;/P&gt;&lt;P&gt;[3] Are they the latest and stable? A more recent package&amp;nbsp;&lt;A href="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-8.0/firmware-imx-8.0.bin"&gt;firmware-imx-8.0.bin&lt;/A&gt;&amp;nbsp;is available, which contains a different&amp;nbsp;&lt;SPAN&gt;vpu_fw_imx6q.bin - which VPU library version is that compatible with?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[4] Will there be any licensing issue if I use the source code and the firmware blob as a reference to port VPU functionality to Windows CE?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help&amp;nbsp;with the above questions - being a linux rookie makes it sometimes very difficult for me to point at the right resources and to find reliable information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Nov 2019 09:26:46 GMT</pubDate>
    <dc:creator>stefano1</dc:creator>
    <dc:date>2019-11-20T09:26:46Z</dc:date>
    <item>
      <title>i.MX6 VPU library source and firmware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013825#M150108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I need to&amp;nbsp;support VPU encoding/decoding on Windows Embedded Compact 2013 (Windows CE).&amp;nbsp;My&amp;nbsp;intention is to port linux code, but I have some problems finding the source code. I'm definitely not a linux build nor Yocto expert, so I'm a little lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The source code for the VPU library is not included in the linux source available on codeaurora - neither in linux-imx nor in linux-lib nor elsewhere I looked at. Furthermore, I need also the binary blob for the VPU firmware (vpu_fw_imx6q.bin and&amp;nbsp;vpu_fw_imx6d.bin), which again seems not to be part of the imx-linux distribution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After&amp;nbsp;much googling I ended up at repository.timesys.com/buildsources,&amp;nbsp;which looks (to me) to "the" repo currently used by the Yocto distributions. There I found the compressed packages for both the&amp;nbsp; VPU library source and the VPU firmare, respectively:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin" title="http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;http://repository.timesys.com/buildsources/i/imx-vpu/imx-vpu-5.4.38/imx-vpu-5.4.38.bin&lt;/A&gt;&amp;nbsp;(latest available)&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin" title="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-5.4/firmware-imx-5.4.bin&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Still, I have some questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1] Is timesys the/an official repository I can safely download up-to-date&amp;nbsp;i.MX linux sources from?&lt;/P&gt;&lt;P&gt;[2] Are those two packages (library 5.4.38 and firmware 5.4) compatible to each other?&lt;/P&gt;&lt;P&gt;[3] Are they the latest and stable? A more recent package&amp;nbsp;&lt;A href="http://repository.timesys.com/buildsources/f/firmware-imx/firmware-imx-8.0/firmware-imx-8.0.bin"&gt;firmware-imx-8.0.bin&lt;/A&gt;&amp;nbsp;is available, which contains a different&amp;nbsp;&lt;SPAN&gt;vpu_fw_imx6q.bin - which VPU library version is that compatible with?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[4] Will there be any licensing issue if I use the source code and the firmware blob as a reference to port VPU functionality to Windows CE?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help&amp;nbsp;with the above questions - being a linux rookie makes it sometimes very difficult for me to point at the right resources and to find reliable information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 09:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013825#M150108</guid>
      <dc:creator>stefano1</dc:creator>
      <dc:date>2019-11-20T09:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 VPU library source and firmware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013826#M150109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we do not support Windows CE on our boards. However, we do have the Linux drivers for the VPU in our BSPs. You could port them to windows on your own.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc?h=imx_4.14.98_2.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc?h=imx_4.14.98_2.0.0_ga"&gt;mxc\drivers - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the inconvenience this may give you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 20:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013826#M150109</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2019-11-26T20:44:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 VPU library source and firmware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013827#M150110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego, thank you for the reply.&lt;/P&gt;&lt;P&gt;Porting to Windows CE is no problem - provided I can find the sources! Unfortunately the link you provided points to the VPU driver, which is&amp;nbsp;just one piece of the puzzle. The VPU driver&amp;nbsp;can be used to access VPU registers, but without a firmware (binary blob) and the related API it's useless.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The point is: where are the (latest stable) VPU firmware binary blob and the&amp;nbsp;companion API source code?&lt;/P&gt;&lt;P&gt;Anyone?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 16:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013827#M150110</guid>
      <dc:creator>stefano1</dc:creator>
      <dc:date>2019-11-27T16:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 VPU library source and firmware</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013828#M150111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, what we have so far is what I sent you. You will need to make the porting of the kernel into the Linux distribution on your own. If you want to use Windows on our boards. I apologize for the inconvenience this may give you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 21:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-VPU-library-source-and-firmware/m-p/1013828#M150111</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2019-11-27T21:53:25Z</dc:date>
    </item>
  </channel>
</rss>