<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ERROR: Function failed: do_rootfs imx6qsabresd yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-rootfs-imx6qsabresd-yocto/m-p/1012047#M149878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using&lt;STRONG&gt; imx-yocto-L4.14.78_1.0.0_ga&lt;/STRONG&gt; on Ubuntu16.04. I finished the build with the commond below&lt;/P&gt;&lt;P&gt;&lt;EM&gt;DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bitbake fsl-image-qt5-validation-imx&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;with some special needs, I changed the source code of busybox-1.27.2, and recompiled.&lt;/P&gt;&lt;P&gt;but there are some errors when do_rootfs&lt;/P&gt;&lt;P&gt;I used the commonds like this:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake -c clean busybox&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake -c compile -f busybox&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake fsl-image-qt5-validation-imx&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error log:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;WARNING: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: Intentionally failing postinstall scriptlets of ['busybox', 'coreutils', 'matchbox-keyboard-im', 'systemd'] to defer them to first boot is deprecated. Please place them into pkg_postinst_ontarget_${PN} ().&lt;BR /&gt;If deferring to first boot wasn't the intent, then scriptlet failure may mean an issue in the recipe, or a regression elsewhere.&lt;BR /&gt;Details of the failure are in /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/temp/log.do_rootfs.&lt;BR /&gt;WARNING: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: [log_check] fsl-image-qt5-validation-imx: found 5 warning messages in the logfile:&lt;BR /&gt;[log_check] warning: %post(busybox-1.27.2-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] warning: %post(coreutils-8.29-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] warning: %post(matchbox-keyboard-im-0.1.1-r0.cortexa9hf_neon) scriptlet failed, exit status 2&lt;BR /&gt;[log_check] warning: %post(systemd-1:237-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] WARNING: Intentionally failing postinstall scriptlets of ['busybox', 'coreutils', 'matchbox-keyboard-im', 'systemd'] to defer them to first boot is deprecated. Please place them into pkg_postinst_ontarget_${PN} ().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: [log_check] fsl-image-qt5-validation-imx: found 2 error messages in the logfile:&lt;BR /&gt;[log_check] update-alternatives: Error: not linking /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel to /bin/busybox.nosuid since /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel exists and is not a link&lt;BR /&gt;[log_check] update-alternatives: Error: not linking /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel to /bin/systemctl since /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel exists and is not a link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/temp/log.do_rootfs.31769&lt;BR /&gt;ERROR: Task (/home/xxx/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb:do_rootfs) failed with exit code '1'&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know how to solve this problem?&lt;/P&gt;&lt;P&gt;Hoping for better guidance.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jan 2020 01:16:39 GMT</pubDate>
    <dc:creator>Gnimis</dc:creator>
    <dc:date>2020-01-15T01:16:39Z</dc:date>
    <item>
      <title>ERROR: Function failed: do_rootfs imx6qsabresd yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-rootfs-imx6qsabresd-yocto/m-p/1012047#M149878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using&lt;STRONG&gt; imx-yocto-L4.14.78_1.0.0_ga&lt;/STRONG&gt; on Ubuntu16.04. I finished the build with the commond below&lt;/P&gt;&lt;P&gt;&lt;EM&gt;DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;bitbake fsl-image-qt5-validation-imx&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;with some special needs, I changed the source code of busybox-1.27.2, and recompiled.&lt;/P&gt;&lt;P&gt;but there are some errors when do_rootfs&lt;/P&gt;&lt;P&gt;I used the commonds like this:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake -c clean busybox&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake -c compile -f busybox&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;bitbake fsl-image-qt5-validation-imx&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error log:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;WARNING: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: Intentionally failing postinstall scriptlets of ['busybox', 'coreutils', 'matchbox-keyboard-im', 'systemd'] to defer them to first boot is deprecated. Please place them into pkg_postinst_ontarget_${PN} ().&lt;BR /&gt;If deferring to first boot wasn't the intent, then scriptlet failure may mean an issue in the recipe, or a regression elsewhere.&lt;BR /&gt;Details of the failure are in /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/temp/log.do_rootfs.&lt;BR /&gt;WARNING: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: [log_check] fsl-image-qt5-validation-imx: found 5 warning messages in the logfile:&lt;BR /&gt;[log_check] warning: %post(busybox-1.27.2-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] warning: %post(coreutils-8.29-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] warning: %post(matchbox-keyboard-im-0.1.1-r0.cortexa9hf_neon) scriptlet failed, exit status 2&lt;BR /&gt;[log_check] warning: %post(systemd-1:237-r0.cortexa9hf_neon) scriptlet failed, exit status 1&lt;BR /&gt;[log_check] WARNING: Intentionally failing postinstall scriptlets of ['busybox', 'coreutils', 'matchbox-keyboard-im', 'systemd'] to defer them to first boot is deprecated. Please place them into pkg_postinst_ontarget_${PN} ().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: [log_check] fsl-image-qt5-validation-imx: found 2 error messages in the logfile:&lt;BR /&gt;[log_check] update-alternatives: Error: not linking /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel to /bin/busybox.nosuid since /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel exists and is not a link&lt;BR /&gt;[log_check] update-alternatives: Error: not linking /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel to /bin/systemctl since /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/rootfs/sbin/runlevel exists and is not a link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-qt5-validation-imx-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/xxx/imx-yocto-bsp/build-x11/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-qt5-validation-imx/1.0-r0/temp/log.do_rootfs.31769&lt;BR /&gt;ERROR: Task (/home/xxx/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb:do_rootfs) failed with exit code '1'&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know how to solve this problem?&lt;/P&gt;&lt;P&gt;Hoping for better guidance.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2020 01:16:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-rootfs-imx6qsabresd-yocto/m-p/1012047#M149878</guid>
      <dc:creator>Gnimis</dc:creator>
      <dc:date>2020-01-15T01:16:39Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR: Function failed: do_rootfs imx6qsabresd yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-rootfs-imx6qsabresd-yocto/m-p/1012048#M149879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the documents as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95046"&gt;busybox on the i.MX6 sabre sd platform in a few commands&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/359546"&gt;https://community.nxp.com/message/359546&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 05:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERROR-Function-failed-do-rootfs-imx6qsabresd-yocto/m-p/1012048#M149879</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-01-16T05:28:00Z</dc:date>
    </item>
  </channel>
</rss>