<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: agetty consuming too much CPU in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/agetty-consuming-too-much-CPU/m-p/1010272#M149611</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not normal and looks strange.&lt;BR /&gt;Possibly there is some another process running from xterm and it is consuming the CPU.&lt;BR /&gt;I can suggest to run the command like "ps auxwwf" to see which processes are running.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Dec 2019 05:35:15 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2019-12-23T05:35:15Z</dc:date>
    <item>
      <title>agetty consuming too much CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/agetty-consuming-too-much-CPU/m-p/1010271#M149610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am running a customized i.MX6ULZ, I connected it by ssh via WiFi, the agetty is the latest CPU consumption process in the first line of top:&lt;/P&gt;&lt;P&gt;PID PPID USER STAT VSZ&amp;nbsp; %VSZ %CPU COMMAND&lt;/P&gt;&lt;P&gt;148 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1500 1%&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 39%&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /sbin/agetty -8 -L ttymxc0 115200 xterm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it normal? If not, how to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- jh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Dec 2019 09:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/agetty-consuming-too-much-CPU/m-p/1010271#M149610</guid>
      <dc:creator>jupiter_hce</dc:creator>
      <dc:date>2019-12-21T09:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: agetty consuming too much CPU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/agetty-consuming-too-much-CPU/m-p/1010272#M149611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not normal and looks strange.&lt;BR /&gt;Possibly there is some another process running from xterm and it is consuming the CPU.&lt;BR /&gt;I can suggest to run the command like "ps auxwwf" to see which processes are running.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2019 05:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/agetty-consuming-too-much-CPU/m-p/1010272#M149611</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-12-23T05:35:15Z</dc:date>
    </item>
  </channel>
</rss>