<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Set asrc input clock to SPDIF_RX_CLK on IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009655#M149565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S/PDIF RX clock is described in sect.50.4.1.8&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82072i9AD7FB8960C3B063/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;some spdif tests which may be useful:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spdif_test/doc?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spdif_test/doc?h=imx_4.19.35_1.1.0"&gt;doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_asrc_test/doc?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_asrc_test/doc?h=imx_4.19.35_1.1.0"&gt;doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 10:16:41 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-11-21T10:16:41Z</dc:date>
    <item>
      <title>Set asrc input clock to SPDIF_RX_CLK on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009654#M149564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on an audio application using an i.MX6ULL and I need to use the hardware ASRC of the processor with the S/PDIF RX clock on the asrc pair input.&lt;/P&gt;&lt;P&gt;The problem I have I that even after the S/PDIF dpll is locked I can't read the rate of the spdif_rx_clk so the pair configuration fails to calculate the input divisor.&lt;/P&gt;&lt;P&gt;In the reference manual I read that after the spdif dpll is locked the received rate is directly generated to spdif_rx_clk. Is that right or are there registers to configure to make it go through to the asrc controller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Manuel BA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 16:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009654#M149564</guid>
      <dc:creator>manuel_soledge</dc:creator>
      <dc:date>2019-11-19T16:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: Set asrc input clock to SPDIF_RX_CLK on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009655#M149565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S/PDIF RX clock is described in sect.50.4.1.8&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82072i9AD7FB8960C3B063/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;some spdif tests which may be useful:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spdif_test/doc?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_spdif_test/doc?h=imx_4.19.35_1.1.0"&gt;doc\mxc_spdif_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_asrc_test/doc?h=imx_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_asrc_test/doc?h=imx_4.19.35_1.1.0"&gt;doc\mxc_asrc_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 10:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009655#M149565</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-11-21T10:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: Set asrc input clock to SPDIF_RX_CLK on IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009656#M149566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your answer, I have been able to recover the RX clock in the asrc module.&lt;BR /&gt;I also have opened another question about the asrc clock sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Manuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 13:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-asrc-input-clock-to-SPDIF-RX-CLK-on-IMX6/m-p/1009656#M149566</guid>
      <dc:creator>manuel_soledge</dc:creator>
      <dc:date>2019-11-21T13:55:53Z</dc:date>
    </item>
  </channel>
</rss>