<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mq Android UVC camera error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android-UVC-camera-error/m-p/1007499#M149281</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Android release notes. The only USB cameras that are supported are the following ones.&lt;/P&gt;&lt;P&gt;Logitech:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;C920&lt;/LI&gt;&lt;LI&gt;C270&lt;/LI&gt;&lt;LI&gt;C525&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that you are using one of those USB cameras.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2019 20:15:07 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2019-11-26T20:15:07Z</dc:date>
    <item>
      <title>imx8mq Android UVC camera error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android-UVC-camera-error/m-p/1007498#M149280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello nxp&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Using USB camera on imx8mq often can't be opened.here is the log info&lt;SPAN&gt;。&lt;/SPAN&gt;our&amp;nbsp;memory 2G Android8.1&lt;SPAN&gt;。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Opening the UVC camera is very slow. It will take a picture automatically for the first time。Android 8.1/9.0 has such problems。Is there any way to solve this problem。 thanks!&lt;/P&gt;&lt;P&gt;E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)&lt;BR /&gt;11-19 03:39:17.088 3069 5335 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)&lt;BR /&gt;11-19 03:39:20.088 3069 5335 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)&lt;BR /&gt;11-19 03:39:20.088 3069 5335 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)&lt;BR /&gt;11-19 03:39:23.088 3069 5335 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)&lt;BR /&gt;11-19 03:39:23.089 3069 5335 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)&lt;BR /&gt;11-19 03:39:26.089 3069 5335 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)&lt;BR /&gt;11-19 03:39:26.089 3069 5335 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)&lt;BR /&gt;11-19 03:39:29.089 3069 5335 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 3000ms (max_buffers 2)&lt;BR /&gt;11-19 03:39:29.089 3069 5335 E Camera3-Device: RequestThread: Can't get output buffer, skipping request: Connection timed out (-110)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 05:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android-UVC-camera-error/m-p/1007498#M149280</guid>
      <dc:creator>bl</dc:creator>
      <dc:date>2019-11-19T05:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android UVC camera error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android-UVC-camera-error/m-p/1007499#M149281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the Android release notes. The only USB cameras that are supported are the following ones.&lt;/P&gt;&lt;P&gt;Logitech:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;C920&lt;/LI&gt;&lt;LI&gt;C270&lt;/LI&gt;&lt;LI&gt;C525&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that you are using one of those USB cameras.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 20:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android-UVC-camera-error/m-p/1007499#M149281</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2019-11-26T20:15:07Z</dc:date>
    </item>
  </channel>
</rss>