<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: CSI input rate on IMX53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222325#M14926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Christophe:&lt;/P&gt;&lt;P&gt;Glad to see it’s helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2013 08:44:15 GMT</pubDate>
    <dc:creator>lily_zhang</dc:creator>
    <dc:date>2013-01-22T08:44:15Z</dc:date>
    <item>
      <title>CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222320#M14921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder what is the real impact of bt mode on csi input rate:&lt;/P&gt;&lt;P&gt;In imx53RM manual at page 546, CSI input rate is said to be 135MP/s in BT1120 an d 67 MP/s in BT656, in 4:2:2.&lt;/P&gt;&lt;P&gt;Now at page 2633 in IPU chapter, CSI input rate is said to be 45Mp/s in 4:2:2, whether the bt mode is, it seems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, what input rate is to be considered ? Is it really possible to reach 135 MP/s in on-the-fly processing with BT1120 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2013 09:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222320#M14921</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2013-01-10T09:29:16Z</dc:date>
    </item>
    <item>
      <title>Re: CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222321#M14922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christophe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum transfer rate must take account the interface bit width.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a YUV4:2:2 (16 bits) format used over a 16 bits interface, the bandwidth will be: 135M/1,5 = 90M Pixels/sec&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a YUV4:2:2 (16 bits) format used over a 8 bits interface, it will take 2 cycles per bit to perform a 16 bits value. The bandwidth will be: 135M/(1,5*2) = 45M Pixels/sec&lt;/P&gt;&lt;P&gt;Rgds&lt;/P&gt;&lt;P&gt;Rogerio&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2013 18:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222321#M14922</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2013-01-18T18:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222322#M14923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rogerio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I agree with you for&amp;nbsp; the secondth point, but not the first:&lt;/P&gt;&lt;P&gt;In 4:2:2, you receive (Y0,Cr0) at n and (Y1,Cb0) at n+1, so 2 samples of 8 bits at each clock period, packed into one 16 bits sample. Moreover, the spec says 135 MP/s in 4:2:2. So the bandwidth must be 135 MP/s or 270 Mo/s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So could you explain the 1,5 factor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds,&lt;/P&gt;&lt;P&gt;Christophe.&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2013 10:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222322#M14923</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2013-01-21T10:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222323#M14924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recommend that you can consider to calculate the required frequency as the followings:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF&lt;/P&gt;&lt;P&gt;Where&lt;/P&gt;&lt;P&gt;• FH = frame height (in pixels)&lt;/P&gt;&lt;P&gt;• FW = Frame width (in pixels)&lt;/P&gt;&lt;P&gt;• fps = frame rate (frames per second)&lt;/P&gt;&lt;P&gt;• BI = typically 35% overhead, should be assumed as 1.35. The actual blanking&lt;/P&gt;&lt;P&gt;intervals are a parameter of the attached device.&lt;/P&gt;&lt;P&gt;• DF = data format, defines the number of cycles needed to send a single pixel.&lt;/P&gt;&lt;P&gt;The number of cycles needed to send a single pixel depends on the interface and the data&lt;/P&gt;&lt;P&gt;format.&lt;/P&gt;&lt;P&gt;Data format examples:&lt;/P&gt;&lt;P&gt;• YUV422 over 16 bit = 1 cycles/pixel&lt;/P&gt;&lt;P&gt;• RGB888 over 8 bit = 1 cycle/pixel&lt;/P&gt;&lt;P&gt;• RGB565 over 16 bit = 2 cycles/pixel&lt;/P&gt;&lt;P&gt;• Bayer/Generic data = 1 cycle/pixel&lt;/P&gt;&lt;P&gt;• YUV422 over 8 bit = 2 cycles/pixel&lt;/P&gt;&lt;P&gt;• BT.656, YUV422 format = 2 cycles/pixel&lt;/P&gt;&lt;P&gt;• BT.1120, YUV422 format = 1 cycle/pixel&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2013 17:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222323#M14924</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-01-21T17:15:56Z</dc:date>
    </item>
    <item>
      <title>Re: CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222324#M14925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now i see where comes the 1,5 factor: ~1/(1-0.35).&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Christophe.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 08:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222324#M14925</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2013-01-22T08:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: CSI input rate on IMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222325#M14926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Christophe:&lt;/P&gt;&lt;P&gt;Glad to see it’s helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 08:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-input-rate-on-IMX53/m-p/222325#M14926</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-01-22T08:44:15Z</dc:date>
    </item>
  </channel>
</rss>