<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Processor CLKIN and CLKOUT pin functionality</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007078#M149239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aurelien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts has an example of driving the CLKO1 pin to feed the OV5640 clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically all you need is to setup the IOMUX for the CLOK1 pin, select the correct parent (24MHz osc in this case) and pass it to the camera node.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Feb 2020 15:34:28 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2020-02-06T15:34:28Z</dc:date>
    <item>
      <title>Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007074#M149235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help to share functionality of processor pins CLKIN1/2 and CLKOUT1/2 (pins H27, J27, H26 and J26). These pins are open (with test point) in EVK also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where can we use these pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 13:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007074#M149235</guid>
      <dc:creator>nija_mankodi</dc:creator>
      <dc:date>2020-01-27T13:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007075#M149236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please resolve this query ASAP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 08:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007075#M149236</guid>
      <dc:creator>nija_mankodi</dc:creator>
      <dc:date>2020-01-29T08:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007076#M149237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nija Mankodi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I would like to confirm that you are referring to the signals of the i.MX8MM Processor. The CLKIN pins allow to feed the main clock instead of SYS_XTAL. If not in use it may be left floating.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The CLKOUT pins can be used to observe internal clocks on a testpoint.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;My apologies for the lack of clarity on the documentation regarding these pins.&lt;BR /&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Feb 2020 00:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007076#M149237</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-02-01T00:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007077#M149238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I am also interested in the answer of how to use it&lt;/P&gt;&lt;P&gt;I am trying to monitor some internal signal of the iMX8MM processor thanks to balls H26=&amp;gt;CLKOUT1 and J26=&amp;gt;CLKOUT2&lt;/P&gt;&lt;P&gt;From my understanding of the reference manual we need to change registers CCM_ANALOG_ANAMIX_PLL_MNIT_CTL 0x30360128 which is page 592 of RM 5.1.8.38 PLL Clock Output for Test Enable and Select Register&lt;/P&gt;&lt;P&gt;The problem is that I don't get any signal from those both pins when writing any value ...&lt;/P&gt;&lt;P&gt;My tests :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;sudo memtool -32 0x30360128=0x1e1&lt;/BLOCKQUOTE&gt;&lt;P&gt;What ever could be the "e" value replaced by anything there is still no signal at the output of CLKOUT1 H26 ball&lt;/P&gt;&lt;P&gt;The value is writen which I confirm in reading then the value :&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;sudo memtool -32 0x30360128 1&lt;BR /&gt;E&lt;BR /&gt;Reading 0x1 count starting at address 0x30360128&lt;BR /&gt;&lt;BR /&gt;0x30360128:&amp;nbsp; 000001E1&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thank you for your support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS : I have updated imx-test to add imx8mm registers here : &lt;A class="link-titled" href="https://github.com/aurelihein/imx-test" title="https://github.com/aurelihein/imx-test"&gt;GitHub - aurelihein/imx-test: Official imx-test(https://source.codeaurora.org/external/imx/imx-test/) adding iMX8MM supp…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Feb 2020 13:39:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007077#M149238</guid>
      <dc:creator>Aurelien_BOUIN</dc:creator>
      <dc:date>2020-02-05T13:39:54Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007078#M149239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aurelien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts has an example of driving the CLKO1 pin to feed the OV5640 clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically all you need is to setup the IOMUX for the CLOK1 pin, select the correct parent (24MHz osc in this case) and pass it to the camera node.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2020 15:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007078#M149239</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2020-02-06T15:34:28Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007079#M149240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fabio,&lt;/P&gt;&lt;P&gt;It seems that you are talking about the pin GPIO1_IO14 (ball : AC9)(unfortunately I don't have test point on this one)&lt;/P&gt;&lt;P&gt;BUT in this thread we are talking about balls H26=&amp;gt;CLKOUT1 and J26=&amp;gt;CLKOUT2&lt;/P&gt;&lt;P&gt;The only documentation I have in reference manual about those pins are :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="RM_CLKOUTX.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102520i3B209165E264D437/image-size/large?v=v2&amp;amp;px=999" role="button" title="RM_CLKOUTX.png" alt="RM_CLKOUTX.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you for your support&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aurelien BOUIN&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 12:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/1007079#M149240</guid>
      <dc:creator>Aurelien_BOUIN</dc:creator>
      <dc:date>2020-02-07T12:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Processor CLKIN and CLKOUT pin functionality</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/2091111#M236914</link>
      <description>&lt;P&gt;Perhaps you should try 0x1d1, 24 MHz input sysclock/2. This one cannot be absent...&lt;/P&gt;&lt;P&gt;I did it with u-boot command:&amp;nbsp;&lt;STRONG&gt;nm.w 30360128 1d1&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I also found clocks on ARM PLL and SYSPLL 1-3.&lt;/P&gt;&lt;P&gt;Please remind that for higher frequency output you should set &lt;STRONG&gt;FSEL_1_FAST_SLEW_RATE&lt;/STRONG&gt; in&amp;nbsp;&lt;STRONG&gt;SW_PAD_CTL_PAD_CLKOUT1 SW PAD&lt;/STRONG&gt; Control Register&lt;/P&gt;</description>
      <pubDate>Sat, 03 May 2025 13:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Processor-CLKIN-and-CLKOUT-pin-functionality/m-p/2091111#M236914</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2025-05-03T13:02:42Z</dc:date>
    </item>
  </channel>
</rss>