<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error with IMAGE_FSTYPES = &amp;quot;sdcard&amp;quot; in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006513#M149171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rutuja Patil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you are using poky 2.6, in this case the problem is that the sdcard format was deprecated on the BSPs in favor of the compressed WIC format. Please use “wic” instead od “sdcard”. It will generate the image in a similar format, but you would need to expand it before copying with dd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Feb 2020 14:27:04 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-02-25T14:27:04Z</dc:date>
    <item>
      <title>Error with IMAGE_FSTYPES = "sdcard"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006512#M149170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While adding&amp;nbsp;IMAGE_FSTYPES = "sdcard", getting error as follow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;buildtools/Yocto2_6_4/build$ bitbake core-image-minimal&lt;BR /&gt;Loading cache: 100% |#######################################################################################################################################| Time: 0:00:00&lt;BR /&gt;Loaded 1415 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |#####################################################################################################################################| Time: 0:00:00&lt;BR /&gt;Parsing of 928 .bb files complete (923 cached, 5 parsed). 1420 targets, 253 skipped, 0 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.40.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "universal"&lt;BR /&gt;TARGET_SYS = "aarch64-fsl-linux"&lt;BR /&gt;MACHINE = "imx8mmevk"&lt;BR /&gt;DISTRO = "fsl-framebuffer"&lt;BR /&gt;DISTRO_VERSION = "2.6"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky &lt;BR /&gt;meta-yocto-bsp &lt;BR /&gt;meta-freescale-distro-thud &lt;BR /&gt;meta-freescale-thud &lt;BR /&gt;meta-spitest = "&amp;lt;unknown&amp;gt;:&amp;lt;unknown&amp;gt;"&lt;/P&gt;&lt;P&gt;WARNING: /home/buildtools/Yocto2_6_4/meta-freescale-thud/recipes-kernel/linux/linux-imx_4.9.123.bb.do_compile is tainted from a forced run | ETA: 0:00:00&lt;BR /&gt;WARNING: /home/buildtools/Yocto2_6_4/meta-freescale-thud/recipes-kernel/linux/linux-imx_4.9.123.bb.do_deploy is tainted from a forced run&lt;BR /&gt;Initialising tasks: 100% |##################################################################################################################################| Time: 0:00:01&lt;BR /&gt;Sstate summary: Wanted 70 Found 0 Missed 70 Current 588 (0% match, 89% complete)&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: core-image-minimal-1.0-r0 do_image_sdcard: Function failed: do_image_sdcard (log file is located at /home/buildtools/Yocto2_6_4/build/tmp/work/imx8mmevk-fsl-linux/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.25836)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/buildtools/Yocto2_6_4/build/tmp/work/imx8mmevk-fsl-linux/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.25836&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing python function set_image_size&lt;BR /&gt;| DEBUG: 9448.400000 = 7268 * 1.300000&lt;BR /&gt;| DEBUG: 9448.400000 = max(9448.400000, 8192)[9448.400000] + 1&lt;BR /&gt;| DEBUG: 9449.000000 = int(9448.400000)&lt;BR /&gt;| DEBUG: 9449 = aligned(9449)&lt;BR /&gt;| DEBUG: returning 9449&lt;BR /&gt;| DEBUG: Python function set_image_size finished&lt;BR /&gt;| DEBUG: Executing shell function do_image_sdcard&lt;BR /&gt;| /home/buildtools/Yocto2_6_4/build/tmp/work/imx8mmevk-fsl-linux/core-image-minimal/1.0-r0/temp/run.do_image_sdcard.25836: line 113: sdcard: command not found&lt;BR /&gt;| WARNING: /home/buildtools/Yocto2_6_4/build/tmp/work/imx8mmevk-fsl-linux/core-image-minimal/1.0-r0/temp/run.do_image_sdcard.25836:1 exit 127 from 'sdcard'&lt;BR /&gt;| ERROR: Function failed: do_image_sdcard (log file is located at /home/buildtools/Yocto2_6_4/build/tmp/work/imx8mmevk-fsl-linux/core-image-minimal/1.0-r0/temp/log.do_image_sdcard.25836)&lt;BR /&gt;ERROR: Task (/home/buildtools/Yocto2_6_4/meta/recipes-core/images/core-image-minimal.bb:do_image_sdcard) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2599 tasks of which 2590 didn't need to be rerun and 1 failed.&lt;BR /&gt;NOTE: Writing buildhistory&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 11:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006512#M149170</guid>
      <dc:creator>rutuja_patil</dc:creator>
      <dc:date>2020-02-24T11:00:01Z</dc:date>
    </item>
    <item>
      <title>Re: Error with IMAGE_FSTYPES = "sdcard"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006513#M149171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rutuja Patil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you are using poky 2.6, in this case the problem is that the sdcard format was deprecated on the BSPs in favor of the compressed WIC format. Please use “wic” instead od “sdcard”. It will generate the image in a similar format, but you would need to expand it before copying with dd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2020 14:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006513#M149171</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-02-25T14:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: Error with IMAGE_FSTYPES = "sdcard"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006514#M149172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. It's working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 05:12:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006514#M149172</guid>
      <dc:creator>rutuja_patil</dc:creator>
      <dc:date>2020-02-26T05:12:54Z</dc:date>
    </item>
    <item>
      <title>Re: Error with IMAGE_FSTYPES = "sdcard"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006515#M149173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/rutuja.patil@kpit.com"&gt;rutuja.patil@kpit.com&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO fsl-framebuffer (Frame Buffer graphics) is not supported on i.MX 8. You can use wayland or xwayland graphics with i.MX8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Radhika Somaiya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2020 11:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-with-IMAGE-FSTYPES-quot-sdcard-quot/m-p/1006515#M149173</guid>
      <dc:creator>radhikasomaiya</dc:creator>
      <dc:date>2020-02-26T11:37:13Z</dc:date>
    </item>
  </channel>
</rss>