<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2S connections to ESAI0 or ESAI1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2S-connections-to-ESAI0-or-ESAI1/m-p/1005987#M149073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sai mapping can be found in IOMUXD Chapter of Reference Manual,&lt;/P&gt;&lt;P&gt;which can be obtained in local marketing office.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2020 10:48:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-01-28T10:48:42Z</dc:date>
    <item>
      <title>I2S connections to ESAI0 or ESAI1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2S-connections-to-ESAI0-or-ESAI1/m-p/1005986#M149072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am trying to work out the pin mapping (if possible) to send I2S audio from ESAI0 or ESAI1 of the i.MX8QM.&lt;BR /&gt;We currently have the I2S slave connected to SAI1, but need this for another audio codec:&lt;BR /&gt;SAI1_TXC ----&amp;gt; I2S_CLK&lt;BR /&gt;SAI1_TXD ----&amp;gt; I2S_TXD&lt;BR /&gt;SAI1_TXFS ---&amp;gt; I2S_WC&lt;BR /&gt;&lt;BR /&gt;Are these 3 I2S signals able to be mapped to ESAI0 or ESAI1 and if so what is the mapping?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 04:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2S-connections-to-ESAI0-or-ESAI1/m-p/1005986#M149072</guid>
      <dc:creator>pbain</dc:creator>
      <dc:date>2020-01-28T04:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: I2S connections to ESAI0 or ESAI1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2S-connections-to-ESAI0-or-ESAI1/m-p/1005987#M149073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sai mapping can be found in IOMUXD Chapter of Reference Manual,&lt;/P&gt;&lt;P&gt;which can be obtained in local marketing office.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 10:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2S-connections-to-ESAI0-or-ESAI1/m-p/1005987#M149073</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-01-28T10:48:42Z</dc:date>
    </item>
  </channel>
</rss>