<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8QXP internal ring oscillator</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004573#M148897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your quick response.&lt;/P&gt;&lt;P&gt;I understood.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;kanou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Feb 2020 05:54:02 GMT</pubDate>
    <dc:creator>mamorukanou</dc:creator>
    <dc:date>2020-02-10T05:54:02Z</dc:date>
    <item>
      <title>i.MX8QXP internal ring oscillator</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004571#M148895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX8QXP Reference Manual chapter 8.1 says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This chapter describes the clocking for all the subsystems in the chip. The chip has three clock sources, two of them originate from external crystals and the third is generated internally by a ring oscillator. The two external crystal oscillators generate 24MHz and 32KHz, and the ring oscillator generates 200MHz. The 32KHz clock can be also sourced from an internal Ring Oscillator, but the frequency will be inaccurate ( +/- 20%) in this case.&lt;BR /&gt;The Ring Oscillator which can generate 200 MHz will be switched off after the initial start up and the 24MHz External Oscillator will take over for the remainder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN title=""&gt;I have questions about this 200MHz clock.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Q1) &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;This PLL is not written in the clock tree figure or table of the manual ? &lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Q2) Is this a provisional PLL until the DIG_PLL0 stabilizes after the power is turned on ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;　　（During normal operation, this 200 MHz ring oscillator is not running.）&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regareds,&lt;/P&gt;&lt;P&gt;kanou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 02:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004571#M148895</guid>
      <dc:creator>mamorukanou</dc:creator>
      <dc:date>2020-02-10T02:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP internal ring oscillator</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004572#M148896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kanou&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Q1) &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;This PLL is not written in the clock tree figure or table of the manual ? &lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;right. Regarding its support please refer to below part of datasheet&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103265i9585447E534AF4F9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&amp;gt;Q2) Is this a provisional PLL until the DIG_PLL0 stabilizes after the power is turned on ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;yes.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&amp;gt;During normal operation, this 200 MHz ring oscillator is not running.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;right.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 05:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004572#M148896</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-02-10T05:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP internal ring oscillator</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004573#M148897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your quick response.&lt;/P&gt;&lt;P&gt;I understood.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;kanou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 05:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-internal-ring-oscillator/m-p/1004573#M148897</guid>
      <dc:creator>mamorukanou</dc:creator>
      <dc:date>2020-02-10T05:54:02Z</dc:date>
    </item>
  </channel>
</rss>