<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: MIPI CSI Line Interrupt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Line-Interrupt/m-p/1004236#M148837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2020 11:24:07 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2020-03-26T11:24:07Z</dc:date>
    <item>
      <title>MIPI CSI Line Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Line-Interrupt/m-p/1004235#M148836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question about the LINE_END interrupt of the MIPI CSI of i.MX8Mmini.&lt;BR /&gt;I set LINE_INTR of "Line Interrupt Ratio" to 0x1.&lt;BR /&gt;In this case, when is the LINE_END interrupt timing of "Interrupt source register 1"?&lt;BR /&gt;Is the size of the received data relevant?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Tetsuya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 15:42:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Line-Interrupt/m-p/1004235#M148836</guid>
      <dc:creator>t-sugiyama</dc:creator>
      <dc:date>2020-03-23T15:42:54Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI Line Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Line-Interrupt/m-p/1004236#M148837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 11:24:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-Line-Interrupt/m-p/1004236#M148837</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2020-03-26T11:24:07Z</dc:date>
    </item>
  </channel>
</rss>