<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How should I understand the IOMUX?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003922#M148779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yan Ding,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an explanation of the 6 available RGPIO2P ports (A-F) on Chapter 40 of the i.MX7ULP Reference Manual, which I understand you have already reviewed. These are designed for general Input Output purposes, but you would need to manage them through software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are SPI and I2C modules that work on hardware so it could be easier to use them before trying to setup these protocols trough software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you haven’t, I would recommend trying the i.MX Pins Tool for i.MX, which may help on configuring your muxing options.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/designs/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX"&gt;https://www.nxp.com/design/designs/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;BR /&gt; Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2020 20:02:11 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-02-11T20:02:11Z</dc:date>
    <item>
      <title>How should I understand the IOMUX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003921#M148778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new in embedded hardware, currently working with i.mx 7 (MCIMX7U5DVK07SC). After reading the "i.MX 7ULP Applications Processor Reference Manual" and the EVK&lt;SPAN class=""&gt;&lt;/SPAN&gt;, I am still confused on the IOMUX function. So far, my understanding is that PTA~PTF ports are function limited GPIOs. The developers need to define the port group (A to F) among Alternative 0 ~ 14.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I look at ALT1: PTA0 is PTA0 ... PTF19 is PTF19. Is this means they can be any low speed bus? I can get 30 I2C bus if necessary? I can get 20 SPI bus if I need? Understand they belongs to different Core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on PCB layout. Due to the board size and siganl layer count reason, I wish to understand the iomux to see how flexible I can define each pin. So that the traces won't be tangled and makes the layout easier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="imx7.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103434iECFC85F8BFC69675/image-size/large?v=v2&amp;amp;px=999" role="button" title="imx7.png" alt="imx7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 04:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003921#M148778</guid>
      <dc:creator>yan_ding</dc:creator>
      <dc:date>2020-02-10T04:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: How should I understand the IOMUX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003922#M148779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yan Ding,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an explanation of the 6 available RGPIO2P ports (A-F) on Chapter 40 of the i.MX7ULP Reference Manual, which I understand you have already reviewed. These are designed for general Input Output purposes, but you would need to manage them through software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are SPI and I2C modules that work on hardware so it could be easier to use them before trying to setup these protocols trough software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you haven’t, I would recommend trying the i.MX Pins Tool for i.MX, which may help on configuring your muxing options.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/designs/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX"&gt;https://www.nxp.com/design/designs/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;BR /&gt; Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2020 20:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003922#M148779</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-02-11T20:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: How should I understand the IOMUX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003923#M148780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you gusarambula.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 14:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-should-I-understand-the-IOMUX/m-p/1003923#M148780</guid>
      <dc:creator>yan_ding</dc:creator>
      <dc:date>2020-02-24T14:03:09Z</dc:date>
    </item>
  </channel>
</rss>