<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Autorun Qt GUI app without login.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Autorun-Qt-GUI-app-without-login/m-p/1002905#M148677</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alexandr Gubanov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One alternative would be adding a script that launches the Qt GUI application on the init.d file inside /etc/init.d&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Mar 2020 21:56:43 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-03-09T21:56:43Z</dc:date>
    <item>
      <title>Autorun Qt GUI app without login.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Autorun-Qt-GUI-app-without-login/m-p/1002904#M148676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need some help.&lt;/P&gt;&lt;P&gt;There is the module on iMX8MQ with Yocto inside. Yocto configured to use xwayland.&lt;/P&gt;&lt;P&gt;There is a Qt GUI application, wich shows some pictures on the screen.&lt;/P&gt;&lt;P&gt;- If I run this app manualy, after login with ROOT, all is OK, it's work fine.&lt;/P&gt;&lt;P&gt;- If I run manualy rc.local with lines for start my app, all is good too.&lt;/P&gt;&lt;P&gt;- But if I reboot module, my app doesn't start. App doesn't start without login. It can't find display.&lt;/P&gt;&lt;P&gt;What should I do to&amp;nbsp;autorun app without login?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2020 16:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Autorun-Qt-GUI-app-without-login/m-p/1002904#M148676</guid>
      <dc:creator>f12358</dc:creator>
      <dc:date>2020-03-07T16:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: Autorun Qt GUI app without login.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Autorun-Qt-GUI-app-without-login/m-p/1002905#M148677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alexandr Gubanov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One alternative would be adding a script that launches the Qt GUI application on the init.d file inside /etc/init.d&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 21:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Autorun-Qt-GUI-app-without-login/m-p/1002905#M148677</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-03-09T21:56:43Z</dc:date>
    </item>
  </channel>
</rss>