<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Linux freez when MIPI &amp; M4 are used in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001541#M148464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SOC operation frequency was limited to 996MHz. &lt;BR /&gt;We are unable to reproduce the problem with SOC frequency of 996MHz. &lt;BR /&gt; &lt;BR /&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jan 2020 11:41:37 GMT</pubDate>
    <dc:creator>urimashiach</dc:creator>
    <dc:date>2020-01-14T11:41:37Z</dc:date>
    <item>
      <title>Linux freez when MIPI &amp; M4 are used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001537#M148460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Hardware: i.MX 7Dual revision 1.2 and 1.3&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Software: Linux, based on NXP &lt;SPAN class=""&gt;4.14.98-2.0.0_ga.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN class=""&gt;Scenario:&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;SPAN class=""&gt;* The M4 core is executing a program that continuously generates UART messages and changing the value of a GPIO.&lt;/SPAN&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* The MIPI display is active.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* The ambient temperature is 45 degrees Celsius.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* The measured temperature, by the A7, is 75C.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;The following command is used to read the A7 temperature:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;# cat /sys/class/thermal/thermal_zone0/temp&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* The Linux get stuck after a few minutes.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* The problem doesn't occur if the M4 or the LVDS is not active.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;* Some SOCs requires a higher temperature to recreate the problem.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Please let me know if additional information is needed.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Uri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2019 10:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001537#M148460</guid>
      <dc:creator>urimashiach</dc:creator>
      <dc:date>2019-11-04T10:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: Linux freez when MIPI &amp; M4 are used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001538#M148461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="border: none; padding: 0in;"&gt;Hi Uri,&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;Have you considered the procedure mentioned on section 2.8.5 of the i.MX Linux Reference Manual document (IMXLXRM Rev. L4.14.98-2.0.0_ga), and also, the notes of Table 10 regarding the proper DTB Description according with the board revision on i.MX Linux Release Notes document (IMXLXRN Rev. L4.14.98-2.0.0_ga)?&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 01:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001538#M148461</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-11-20T01:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: Linux freez when MIPI &amp; M4 are used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001539#M148462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please provide links to the documents from your reply:&lt;/P&gt;&lt;P&gt;* MXLXRM Rev. L4.14.98-2.0.0_ga&lt;/P&gt;&lt;P&gt;* IMXLXRN Rev. L4.14.98-2.0.0_ga&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Uri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 08:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001539#M148462</guid>
      <dc:creator>urimashiach</dc:creator>
      <dc:date>2019-11-21T08:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: Linux freez when MIPI &amp; M4 are used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001540#M148463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="border: none; padding: 0in;"&gt;Hi Uri,&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;These documents are part of the Linux BSP documentation package, available on the following link:&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga"&gt;https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 21:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001540#M148463</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-11-21T21:40:14Z</dc:date>
    </item>
    <item>
      <title>Re: Linux freez when MIPI &amp; M4 are used</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001541#M148464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SOC operation frequency was limited to 996MHz. &lt;BR /&gt;We are unable to reproduce the problem with SOC frequency of 996MHz. &lt;BR /&gt; &lt;BR /&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2020 11:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-freez-when-MIPI-M4-are-used/m-p/1001541#M148464</guid>
      <dc:creator>urimashiach</dc:creator>
      <dc:date>2020-01-14T11:41:37Z</dc:date>
    </item>
  </channel>
</rss>