<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How Yocto Linux handle the user data section during the flashing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-Yocto-Linux-handle-the-user-data-section-during-the-flashing/m-p/1000806#M148397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using IMX8mini EVK, flashing the whole system via UUU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But after flashing, all user-data would be erased as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm wondering if we can have similar behavior as Android's userdata partiion, so flashing would no erase user's data. Can IMX8mini Yocto Linux support this? And if it does, how to ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2020 01:35:09 GMT</pubDate>
    <dc:creator>13614278</dc:creator>
    <dc:date>2020-03-23T01:35:09Z</dc:date>
    <item>
      <title>How Yocto Linux handle the user data section during the flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Yocto-Linux-handle-the-user-data-section-during-the-flashing/m-p/1000806#M148397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using IMX8mini EVK, flashing the whole system via UUU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But after flashing, all user-data would be erased as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm wondering if we can have similar behavior as Android's userdata partiion, so flashing would no erase user's data. Can IMX8mini Yocto Linux support this? And if it does, how to ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 01:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Yocto-Linux-handle-the-user-data-section-during-the-flashing/m-p/1000806#M148397</guid>
      <dc:creator>13614278</dc:creator>
      <dc:date>2020-03-23T01:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: How Yocto Linux handle the user data section during the flashing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-Yocto-Linux-handle-the-user-data-section-during-the-flashing/m-p/1000807#M148398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;A _jive_internal="true" data-content-finding="Community" data-userid="349686" data-username="13614278@qq.com" href="https://community.nxp.com/people/13614278@qq.com"&gt;Songxiang&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See below, please!&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;1. when you program images to eMMC on board for the first time, Commands for partition must be run in uuu script.&lt;/P&gt;&lt;P&gt;2. when you update images later, if you don't want data lost, you should comment "create partition" commands in uuu script.&lt;BR /&gt;you can try it, please!&lt;/P&gt;&lt;P&gt;--------------------&lt;/P&gt;&lt;P&gt;Chinse:&lt;/P&gt;&lt;P&gt;1. 第一次烧写image的时候，你必须要运行完整的脚本中的命令，因为EMMC/SD卡需要分区。&lt;/P&gt;&lt;P&gt;2. 第二次或者以后更新image的时候，如果你需要保留数据，那么你可以注释掉脚本中的分区命令。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;试试看！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;附件里是我使用过的uuu 脚本，给你参考。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 02:49:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-Yocto-Linux-handle-the-user-data-section-during-the-flashing/m-p/1000807#M148398</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-03-23T02:49:44Z</dc:date>
    </item>
  </channel>
</rss>