<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux kernel image and optee image UUU in iMX8M Mini in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-image-and-optee-image-UUU-in-iMX8M-Mini/m-p/999604#M148244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded L4.14.98_2.0.0_ga_images_MX8MMEVK and I am using the example&amp;nbsp;example_kernel_emmc, and I see that it uses _Image and uTee.tar. Where are those files?&lt;BR /&gt;can i use Image-imx8mmevk.bin as _Image? Where can I get uTee.tar?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone explain to me where to get these files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Feb 2020 13:58:46 GMT</pubDate>
    <dc:creator>inigovicentewal</dc:creator>
    <dc:date>2020-02-07T13:58:46Z</dc:date>
    <item>
      <title>Linux kernel image and optee image UUU in iMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-image-and-optee-image-UUU-in-iMX8M-Mini/m-p/999604#M148244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded L4.14.98_2.0.0_ga_images_MX8MMEVK and I am using the example&amp;nbsp;example_kernel_emmc, and I see that it uses _Image and uTee.tar. Where are those files?&lt;BR /&gt;can i use Image-imx8mmevk.bin as _Image? Where can I get uTee.tar?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone explain to me where to get these files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 13:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-image-and-optee-image-UUU-in-iMX8M-Mini/m-p/999604#M148244</guid>
      <dc:creator>inigovicentewal</dc:creator>
      <dc:date>2020-02-07T13:58:46Z</dc:date>
    </item>
    <item>
      <title>Re: Linux kernel image and optee image UUU in iMX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-image-and-optee-image-UUU-in-iMX8M-Mini/m-p/999605#M148245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes you can use Image-imx8mmevk.bin as _Image, for OP-TEE it doesn't come in the demo image we provide, it needs to be compiled by customers.&lt;/P&gt;&lt;P&gt;Please take a look to the i.MX Yocto Project User's Guide, section 5.6.10 OP-TEE enablement, you can download documentation from here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3FcolCode%3Dimx-yocto-L4.14.98_2.0.0_ga"&gt;Linux L4.14.98_2.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't want/need to use Optee you can always use uuu.auto to flash the demo image, uboot and rootfs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Aldo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2020 21:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-image-and-optee-image-UUU-in-iMX8M-Mini/m-p/999605#M148245</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2020-02-11T21:40:51Z</dc:date>
    </item>
  </channel>
</rss>